[#4859] netperf-x86 compiling fails with gcc-4.3.2

Document created by Aaronwu Employee on Aug 30, 2013
Version 1Show Document
  • View in full screen mode

[#4859] netperf-x86 compiling fails with gcc-4.3.2

Submitted By: Michael Hennerich

Open Date

2009-02-05 04:40:33     Close Date

2010-02-22 10:37:20

Priority:

Very Low     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

uClinux-dist applications     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

N/A

Uboot version or rev.:

    Toolchain version or rev.:

hostcc: gcc-4.3.2

App binary format:

N/A     

Summary: netperf-x86 compiling fails with gcc-4.3.2

Details:

 

michael@mhenneri-D02:~/devel/svn/uclinux-dist-trunk_3/user/blkfin-test/netperf-x86> gcc -v

Using built-in specs.

Target: x86_64-suse-linux

Configured with: ../configure --prefix=/usr --infodir=/usr/share/info --mandir=/usr/share/man --libdir=/usr/lib64 --libexecdir=/usr/lib64 --enable-languages=c,c++,objc,fortran,obj-c++,java,ada --enable-checking=release --with-gxx-include-dir=/usr/include/c++/4.3 --enable-ssp --disable-libssp --with-bugurl=  bugs.opensuse.org/ --with-pkgversion='SUSE Linux' --disable-libgcj --disable-libmudflap --with-slibdir=/lib64 --with-system-zlib --enable-__cxa_atexit --enable-libstdcxx-allocator=new --disable-libstdcxx-pch --enable-version-specific-runtime-libs --program-suffix=-4.3 --enable-linux-futex --without-system-libunwind --with-cpu=generic --build=x86_64-suse-linux

Thread model: posix

gcc version 4.3.2 [gcc-4_3-branch revision 141291] (SUSE Linux)

 

michael@mhenneri-D02:~/devel/svn/uclinux-dist-trunk_3/user/blkfin-test/netperf-x86> ./configure

checking build system type... x86_64-unknown-linux-gnu

checking host system type... x86_64-unknown-linux-gnu

checking target system type... x86_64-unknown-linux-gnu

checking for a BSD-compatible install... /usr/bin/install -c

 

--snip--

 

checking for in_port_t... no

configure: error: Failed to get size of sin_port in struct sockaddr_in.

 

 

Same issue as described here:

  bugs.gentoo.org/126334

 

-Michael

 

Follow-ups

 

--- Mike Frysinger                                           2009-02-05 10:39:17

those netperf dirs are a complete mess (they include prebuilt binaries) and

afaik, the testing code uses it.  in other words, i'm not about to touch it

without throwing it all away ;).

 

--- Michael Hennerich                                        2009-02-09 03:54:09

Well - throwing it all away is an option for me too.

-Michael

 

--- Michael Hennerich                                        2010-02-22 10:36:31

close it

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes