[#4824] AD1980 AC97 reset failed in BF527-EZKIT

Document created by Aaronwu Employee on Aug 30, 2013
Version 1Show Document
  • View in full screen mode

[#4824] AD1980 AC97 reset failed in BF527-EZKIT

Submitted By: Vivi Li

Open Date

2009-01-20 05:15:05     Close Date

2009-02-04 05:43:03

Priority:

Medium     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

EZKIT Lite

Processor:

BF527     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Not reproducible

Uboot version or rev.:

    Toolchain version or rev.:

toolchain 4.1-2008_Dec_12

App binary format:

N/A     

Summary: AD1980 AC97 reset failed in BF527-EZKIT

Details:

 

AD1980 AC97 reset failed in BF527-EZKIT.

 

--

Linux version 2.6.28-ADI-2009R1-pre-svn6027 (test@uboot30-527ezkit) (gcc version 4.1.2 (ADI svn)) #9

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00139750

  rodata    = 0x00139750-0x0019a1f4

  bss       = 0x0019a200-0x001a986c

  data      = 0x001a986c-0x001bc000

    stack   = 0x001ba000-0x001bc000

  init      = 0x001bc000-0x007b8000

  available = 0x007b8000-0x03dff000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 9

Blackfin support (C) 2004-2008 Analog Devices, Inc.

Compiled for ADSP-BF527 Rev 0.0

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 15747

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart1,57600 consolf

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 55000k/65536k RAM, (6128k init code, 1249k kernel code, 523k data, 2048k dma, 584)

Calibrating delay loop... 1044.48 BogoMIPS (lpj=2088960)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

PDA for CPU0 reserved at 0019b130

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

ezkit_init(): registering device resources

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

musb_hdrc: version 6.0, pio, host, debug=0

musb_hdrc: USB Host mode controller at ffc03800 using PIO, IRQ 59

musb_hdrc musb_hdrc.0: MUSB HDRC host driver

musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 107

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-otp: initialized

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART

brd: module loaded

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:03, irq=-1, mdc_clk=2500000Hz(mdc_d)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

m25p80 spi0.1: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x00000000-0x00040000 : "bootloader(spi)"

0x00040000-0x00200000 : "linux kernel(spi)"

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma c7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

hid_tmff: Unknown symbol _input_ff_create_memless

usbcore: registered new interface driver usbhid

usbhid: v2.6:USB HID core driver

Advanced Linux Sound Architecture Driver Version 1.0.18rc3.

ASoC version 0.13.2

dma rx:3 tx:4, err irq:15, regs:ffc00800

AD1980 SoC Audio Codec

dma_alloc_init: dma_page @ 0x03a9a000 - 512 pages at 0x03e00000

asoc: AC97 <-> bf5xx-ac97 mapping ok

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

AD1980 AC97 reset failed

AC97 link error

soc-audio: probe of soc-audio failed with error -5

ALSA device list:

  No soundcards found.

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1974-09-17 23:56:30 UTC (148694190)

IP-Config: Gateway not on directly connected network.

Freeing unused kernel memory: 6128k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

kf 8a.   :     _a88P         For further infPHmatY: 0 ch:03 out- Lin_/"k i_: s Up 8 P|-      1   0-l

  n.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.2 (2009-01-20 15:36:30 GMT) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/>

--

 

Follow-ups

 

--- Cliff Cai                                                2009-01-21 02:46:09

It should be OK.Actually,the interface labled "sport0" is sport0A,

So,you should select PORTG for sport0A,and turn sw17 sw20 all off.

 

Cliff

 

--- Vivi Li                                                  2009-02-04 05:43:03

OK now. Close it.

Thanks!

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes