[#4790] bf533-stamp/ezkit can't boot up with earlyprintk kernel

Document created by Aaronwu Employee on Aug 30, 2013
Version 1Show Document
  • View in full screen mode

[#4790] bf533-stamp/ezkit can't boot up with earlyprintk kernel

Submitted By: Vivi Li

Open Date

2009-01-09 05:30:29     Close Date

2009-01-12 21:48:13

Priority:

Medium     Assignee:

Robin Getz

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

STAMP

Processor:

BF533     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Assigned (Not Start)

Uboot version or rev.:

U-Boot 2008.10     Toolchain version or rev.:

gcc 4.1-2008_Dec_1

App binary format:

N/A     

Summary: bf533-stamp/ezkit can't boot up with earlyprintk kernel

Details:

 

bf533-stamp/ezkit can't boot up in U-Boot 2008.10 with earlyprintk kernel.

 

But it can boot up from 2008R1.5 u-boot. Meanwhile, other latest kernels can boot in U-Boot 2008.10.

 

Bellow is the log:

--

U-Boot 2008.10-svn1496 (ADI-2009R1-pre) (Dec  3 2008 - 12:16:52)

 

CPU:   ADSP bf533-0.3 (Detected Rev: 0.3)

Board: ADI BF533 Stamp board

       Support:   blackfin.uclinux.org/

Clock: VCO: 497.664 MHz, Core: 497.664 MHz, System: 99.532 MHz

RAM:   128 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   MAC:   F2:06:01:61:68:B5

Hit any key to stop autoboot:  0

bfin>

bfin> tftp 0x1000000 linux

Using MAC Address F2:06:01:61:68:B5

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'linux'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         ##################

done

Bytes transferred = 5022173 (4ca1dd hex)

bfin> boote

Loading phdr 0 to 0x00001000 (1413156 bytes)

Loading phdr 1 to 0x00168458 (2999716 bytes)

Loading phdr 2 to 0x004449fc (6692 bytes)

Loading phdr 3 to 0x00446420 (192 bytes)

## Starting application at 0x00182cc0 ...

--

 

Follow-ups

 

--- Robin Getz                                               2009-01-09 15:09:09

That is because you need to boot the uImage.

 

Please stop using elf files.

 

-Robin

 

--- Vivi Li                                                  2009-01-12 21:48:13

We are using uImage now.

Close this bug.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes