[#4782] YAFFS build fails after kernel update.

Document created by Aaronwu Employee on Aug 30, 2013
Version 1Show Document
  • View in full screen mode

[#4782] YAFFS build fails after kernel update.

Submitted By: Bryan Wu

Open Date

2009-01-08 03:59:28     Close Date

2009-01-08 05:11:38

Priority:

Medium     Assignee:

Bryan Wu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

snaps     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

trunk

App binary format:

N/A     

Summary: YAFFS build fails after kernel update.

Details:

 

  CC [M]  fs/smbfs/file.o

fs/yaffs2/yaffs_fs.c:234: error: unknown field ‘prepare_write’ specified in initializer

fs/yaffs2/yaffs_fs.c:234: warning: initialization from incompatible pointer type

fs/yaffs2/yaffs_fs.c:235: error: unknown field ‘commit_write’ specified in initializer

fs/yaffs2/yaffs_fs.c:235: warning: initialization from incompatible pointer type

make[3]: *** [fs/yaffs2/yaffs_fs.o] Error 1

make[2]: *** [fs/yaffs2] Error 2

 

-Bryan

 

Follow-ups

 

--- Bryan Wu                                                 2009-01-08 05:11:38

fixed now

 

-bryan

 

--- jitendra kumar                                           2009-06-11 23:45:32

May I know the fix for this error?

 

--- Mike Frysinger                                           2009-06-12 00:03:44

this only affected versions of svn that you should not be using in the first

place

 

--- jitendra kumar                                           2009-06-12 00:08:24

Wow, that was an unexpectedly quick reply.

Sorry, didn't get that, do you mean the 2.6.28 kernel? because I have the final

release of that from kernel.org.

 

--- Mike Frysinger                                           2009-06-12 03:45:29

kernels from kernel.org arent supported

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes