[#4734] traps test case 19 for exception 0x2d fails

Document created by Aaronwu Employee on Aug 30, 2013
Version 1Show Document
  • View in full screen mode

[#4734] traps test case 19 for exception 0x2d fails

Submitted By: Mingquan Pan

Open Date

2008-12-21 23:37:44     Close Date

2009-02-10 01:30:49

Priority:

Medium High     Assignee:

Bernd Schmidt

Robin Getz

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

Nov 11

App binary format:

N/A     

Summary: traps test case 19 for exception 0x2d fails

Details:

 

traps test case 19 for exception 0x2d fails on trunk,check in between svn 5855 to 5863 due to this.

 

Running test 19 for exception 0x2d: Instruction fetch multiple CPLB hits - Jump to zero

... Instruction fetch CPLB miss

- CPLB miss on an instruction fetch.

Deferred Exception context

CURRENT PROCESS:

COMM=traps_test PID=321

CPU = 0

TEXT = 0x00670040-0x00674660        DATA = 0x00674664-0x00676574

BSS = 0x00676574-0x00676814  USER-STACK = 0x00677f78

 

return address: [0x72742f2e]; contents of:

0x72742f00:  ????  ????  ????  ????  ????  ????  ????  ????

0x72742f10:  ????  ????  ????  ????  ????  ????  ????  ????

0x72742f20:  ????  ????  ????  ????  ????  ????  ???? [????]

0x72742f30:  ????  ????  ????  ????  ????  ????  ????  ????

 

SEQUENCER STATUS:               Not tainted

SEQSTAT: 0006202c  IPEND: 0030  SYSCFG: 0006

  EXCAUSE   : 0x2c

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x03210000> /* kernel dynamic memory */

RETX: <0x00000480> /* Maybe fixed code section */

RETS: <0x00000000> /* Maybe null pointer? */

PC  : <0x72742f2e> /* kernel dynamic memory */

DCPLB_FAULT_ADDR: <0x0320fffc> /* kernel dynamic memory */

ICPLB_FAULT_ADDR: <0x72742f2e> /* kernel dynamic memory */

 

PROCESSOR STATE:

R0 : 00417f7c    R1 : 00000000    R2 : 004167f0    R3 : 00000002

R4 : 004103b4    R5 : 00000000    R6 : 00000000    R7 : 00000000

P0 : 00674638    P1 : 0067464a    P2 : 00000000    P3 : 004167f0

P4 : 00000002    P5 : 00677f9c    FP : 74736574    SP : 0320ff24

LB0: 00747365    LT0: 6172742e    LC0: 6e696c3d

LB1: 00000001    LT1: 745f7370    LC1: 2e007875

B0 : 752f3a6e    L0 : 2f3a6e69    M0 : 69622f3d    I0 : 00393100

B1 : 732f7273    L1 : 2f727375    M1 : 68732f6e    I1 : 454d4f48

B2 : 006e6962    L2 : 3a6e6962    M2 : 54415000    I2 : 53002f3d

B3 : 4d524554    L3 : 6962732f    M3 : 622f3d48    I3 : 4c4c4548

A0.w: 00000000   A0.x: ffffffb3   A1.w: 00677fac   A1.x: ffffffc1

USP : 00677fa9  ASTAT: 00677fe4

 

No trace since you do not have CONFIG_DEBUG_BFIN_NO_KERN_HWTRACE enabled

 

Userspace Stack

Stack info:

SP: [0x00677fa9] <0x00677fa9> [ traps_test + 0x7fa9 ]

Memory from 0x00677fa0 to 00678000

00677fa0: 5f737061  74736574  00393100  454d4f48  53002f3d  4c4c4548  69622f3d  68732f6e

00677fc0: 54415000  622f3d48  2f3a6e69  2f727375  3a6e6962  6962732f  752f3a6e  732f7273

00677fe0: 006e6962  4d524554  6e696c3d  2e007875  6172742f  745f7370  00747365  00000000

00678000: 69666b63

Return addresses in stack:

FAIL (test failed, but not with the right signal)

        (We expected 11 'Segmentation fault' but instead we got 7 'Bus error')

 

 

Follow-ups

 

--- Mingquan Pan                                             2008-12-30 04:45:41

And also when this bug happens, the uclinux-dist checkins change from 7453 to

7458 (in Dec 12-13).

 

--- Robin Getz                                               2009-01-05 13:30:23

The test case:

 

void jump_to_zero(void)

{

        int (*foo)(void);

        int i;

        i=0x0;

        foo = (void *)i;

        (*foo)();

}

 

should jump to zero, and cause a double icplb fault - but this is getting a not

installed error.

 

This makes sense on a MPU kernel - but on a noMMU kernel.

 

Can you print out /proc/cpuinfo and /proc/cplb

 

Thanks

 

--- Mingquan Pan                                             2009-01-14 03:54:08

It is:

 

root:/bin>

root:/bin> cat /proc/cpuinfo

processor       : 0

vendor_id       : Analog Devices

cpu family      : 0x27c8

model name      : ADSP-BF537 500(MHz CCLK) 100(MHz SCLK) (mpu off)

stepping        : 2

cpu MHz         : 500.000/100.000

bogomips        : 995.32

Calibration     : 497664000 loops

cache size      : 16 KB(L1 icache) 32 KB(L1 dcache-wt) 0 KB(L2 cache)

dbank-A/B       : cache/cache

icache setup    : 4 Sub-banks/4 Ways, 32 Lines/Way

dcache setup    : 2 Super-banks/4 Sub-banks/2 Ways, 64 Lines/Way

board name      : ADI BF537-STAMP

board memory    : 65536 kB (0x00000000 -> 0x04000000)

kernel memory   : 57336 kB (0x00001000 -> 0x037ff000)

 

root:/bin> cat /proc/cplbinfo/cpu0/

/proc/cplbinfo/cpu0/dcplb  /proc/cplbinfo/cpu0/icplb

root:/bin> cat /proc/cplbinfo/cpu0/dcplb

DCPLBs are enabled: 0x100f

Index   Address         Data    Size    U/RD    U/WR    S/WR    Switch

0       0x00000000      00083   1K      N       N       N       N

1       0x00000000      3d09d   4M      Y       Y       Y       N

2       0x00400000      3d09d   4M      Y       Y       Y       N

3       0xff800000      3009f   4M      Y       Y       Y       N

4       0x00800000      3d09d   4M      Y       Y       Y       Y

5       0x03700000      2d09d   1M      Y       Y       Y       Y

6       0x03600000      2d09d   1M      Y       Y       Y       Y

7       0x03400000      2d09d   1M      Y       Y       Y       Y

8       0x03500000      2d09d   1M      Y       Y       Y       Y

9       0x03000000      3d09d   4M      Y       Y       Y       Y

10      0x03c00000      3009d   4M      Y       Y       Y       Y

11      0x00000000      00000   1K      N       N       N       Y

12      0x00000000      00000   1K      N       N       N       Y

13      0x00000000      00000   1K      N       N       N       Y

14      0x00000000      00000   1K      N       N       N       Y

15      0x00000000      00000   1K      N       N       N       Y

root:/bin> cat /proc/cplbinfo/cpu0/icplb

ICPLBs are enabled: 0x7

Index   Address         Data    Size    U/RD    U/WR    S/WR    Switch

0       0x00000000      31205   4M      Y       N       N       N

1       0x00400000      31205   4M      Y       N       N       N

2       0xffa00000      30007   4M      Y       N       N       N

3       0x03000000      31205   4M      Y       N       N       Y

4       0x03700000      21205   1M      Y       N       N       Y

5       0x00000000      00000   1K      N       N       N       Y

6       0x00000000      00000   1K      N       N       N       Y

7       0x00000000      00000   1K      N       N       N       Y

8       0x00000000      00000   1K      N       N       N       Y

9       0x00000000      00000   1K      N       N       N       Y

10      0x00000000      00000   1K      N       N       N       Y

11      0x00000000      00000   1K      N       N       N       Y

12      0x00000000      00000   1K      N       N       N       Y

13      0x00000000      00000   1K      N       N       N       Y

14      0x00000000      00000   1K      N       N       N       Y

15      0x00000000      00000   1K      N       N       N       Y

root:/bin>

 

--- Robin Getz                                               2009-01-14 07:50:19

OK - this _is_ a MPU kernel, and there isn't a dup 1k CPLB installed at zero.

 

I'll check with Bernd to see if this is the correct setup.

 

-Robin

 

--- Robin Getz                                               2009-01-14 18:39:42

Bernd said - no -- this is not correct...

 

So, either he or I will fix.

 

--- Bernd Schmidt                                            2009-01-29 14:09:30

I've committed a fix, so closing.

 

Gforge requires me to fill in meaningless fields to close the bug.  This is

annoying.

 

--- Sonic Zhang                                              2009-02-01 21:26:57

The "Found In Release:*" field should be filled in with current

release candicated "2009R1-RC1". The "Processor:" field

should be "ALL" for this bug.

 

From now on, all these information should be filled in when a new bug is

filed.

 

--- Mingquan Pan                                             2009-02-04 03:25:51

It is strange that this is fixed on one board of bf537 stamp. While on some

other 537 board and bf527 ezkit board, it would stuck at  case 19 for quite a

while until 50 minutes timeout:

 

PASS (test failed as expected by signal 7: Bus error)^M

Pass_num is 18 .^M

Running test 19 for exception 0x2d: Instruction fetch multiple CPLB hits - Jump

to zero^M

... ^M

Running test 19 for exception 0x2d: Instruction fetch multiple CPLB hits - Jump

to zero^M

...

Case 1 ...FAIL

 

root:/bin> cat /proc/cpuinfo

processor       : 0

vendor_id       : Analog Devices

cpu family      : 0x27c8

model name      : ADSP-BF537 500(MHz CCLK) 100(MHz SCLK) (mpu off)

stepping        : 2

cpu MHz         : 500.000/100.000

bogomips        : 995.32

Calibration     : 497664000 loops

cache size      : 16 KB(L1 icache) 32 KB(L1 dcache-wt) 0 KB(L2 cache)

dbank-A/B       : cache/cache

icache setup    : 4 Sub-banks/4 Ways, 32 Lines/Way

dcache setup    : 2 Super-banks/4 Sub-banks/2 Ways, 64 Lines/Way

board name      : ADI BF537-STAMP

board memory    : 65536 kB (0x00000000 -> 0x04000000)

kernel memory   : 57336 kB (0x00001000 -> 0x037ff000)

 

root:/bin> cd

root:/>  cat /proc/cplbinfo/cpu0/dcplb

DCPLBs are enabled: 0x100f

Index   Address         Data    Size    U/RD    U/WR    S/WR    Switch

0       0x00000000      00083   1K      N       N       N       N

1       0x00000000      3d09d   4M      Y       Y       Y       N

2       0x00400000      3d09d   4M      Y       Y       Y       N

3       0xff800000      3009f   4M      Y       Y       Y       N

4       0x00800000      3d09d   4M      Y       Y       Y       Y

5       0x03700000      2d09d   1M      Y       Y       Y       Y

6       0x03600000      2d09d   1M      Y       Y       Y       Y

7       0x03400000      2d09d   1M      Y       Y       Y       Y

8       0x03500000      2d09d   1M      Y       Y       Y       Y

9       0x03000000      3d09d   4M      Y       Y       Y       Y

10      0x03c00000      3009d   4M      Y       Y       Y       Y

11      0x00000000      00000   1K      N       N       N       Y

12      0x00000000      00000   1K      N       N       N       Y

13      0x00000000      00000   1K      N       N       N       Y

14      0x00000000      00000   1K      N       N       N       Y

15      0x00000000      00000   1K      N       N       N       Y

root:/> cat /proc/cplbinfo/cpu0/icplb

ICPLBs are enabled: 0x7

Index   Address         Data    Size    U/RD    U/WR    S/WR    Switch

0       0x00000000      31205   4M      Y       N       N       N

1       0x00400000      31205   4M      Y       N       N       N

2       0xffa00000      30007   4M      Y       N       N       N

3       0x03000000      31205   4M      Y       N       N       Y

4       0x00800000      31205   4M      Y       N       N       Y

5       0x00000000      00000   1K      N       N       N       Y

6       0x00000000      00000   1K      N       N       N       Y

7       0x00000000      00000   1K      N       N       N       Y

8       0x00000000      00000   1K      N       N       N       Y

9       0x00000000      00000   1K      N       N       N       Y

10      0x00000000      00000   1K      N       N       N       Y

11      0x00000000      00000   1K      N       N       N       Y

12      0x00000000      00000   1K      N       N       N       Y

13      0x00000000      00000   1K      N       N       N       Y

14      0x00000000      00000   1K      N       N       N       Y

15      0x00000000      00000   1K      N       N       N       Y

root:/>

root:/> version

kernel:    Linux release 2.6.28-ADI-2009R1-pre-svn6043, build #42 Tue Feb 3

05:03:24 CST 2009

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-7698, build #510 Tue Feb 3 05:00:34 CST 2009

 

 

While on bf548-ezkit, it outputs different:

Running test 19 for exception 0x2d: Instruction fetch multiple CPLB hits - Jump

to zero

...

Running test 19 for exception 0x2d: Instruction fetch multiple CPLB hits - Jump

to zero

... Undefined instruction

- May be used to emulate instructions that are not defined for

   a particular processor implementation.

Deferred Exception context

CURRENT PROCESS:

COMM=traps_test PID=352

CPU = 0

TEXT = 0x008f8040-0x008fc640        DATA = 0x008fc644-0x008fe544

BSS = 0x008fe544-0x008fe7e4  USER-STACK = 0x008fff78

 

return address: [0x00000080]; contents of:

0x00000060:  ????  ????  ????  ????  ????  ????  ????  ????

0x00000070:  ????  ????  ????  ????  ????  ????  ????  ????

0x00000080: [????] ????  ????  ????  ????  ????  ????  ????

0x00000090:  ????  ????  ????  ????  ????  ????  ????  ????

 

SEQUENCER STATUS:               Not tainted

SEQSTAT: 00062021  IPEND: 0030  SYSCFG: 0006

  EXCAUSE   : 0x21

  interrupts disabled

  physical IVG5 asserted : <0xffa00b24> { _evt_ivhw + 0x0 }

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x008d6000> /* kernel dynamic memory */

RETX: <0x00000480> /* Maybe fixed code section */

RETS: <0x008f82b4> [ traps_test + 0x274 ]

PC  : <0x00000080> /* Maybe null pointer? */

DCPLB_FAULT_ADDR: <0x008ffeac> [ traps_test + 0x7eac ]

ICPLB_FAULT_ADDR: <0x00000080> /* Maybe null pointer? */

 

PROCESSOR STATE:

R0 : 00000000    R1 : 00000013    R2 : 008fdaf0    R3 : 00000008

R4 : 008f83b4    R5 : 00000002    R6 : 008fe7c0    R7 : 00000000

P0 : 000000a2    P1 : 0000001f    P2 : 00000000    P3 : 008fff7c

P4 : 008fe540    P5 : 008fc644    FP : 008ffeb4    SP : 008d5f24

LB0: 008f98d3    LT0: 008f98d2    LC0: 00000000

LB1: 008fa1e7    LT1: 008fa1e0    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 008ffc64

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 008b8004

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000

USP : 008ffea0  ASTAT: 02002020

 

Hardware Trace:

   0 Target : <0x00004abc> { _trap_c + 0x0 }

     Source : <0xffa005e2> { _exception_to_level5 + 0x9e } CALL pcrel

   1 Target : <0xffa00544> { _exception_to_level5 + 0x0 }

     Source : <0xffa00416> { _bfin_return_from_exception + 0x6 } RTX

   2 Target : <0xffa00410> { _bfin_return_from_exception + 0x0 }

     Source : <0xffa0049e> { _ex_trap_c + 0x66 } JUMP.S

   3 Target : <0xffa00438> { _ex_trap_c + 0x0 }

     Source : <0xffa0066e> { _trap + 0x2a } JUMP (P4)

   4 Target : <0xffa00644> { _trap + 0x0 }

     Source : <0x0000007e> /* Maybe null pointer? */

   5 Target : <0x00000000> /* Maybe null pointer? */

     Source : <0x008f82b2> [ traps_test + 0x272 ] CALL (P2)

   6 Target : <0x008f82a4> [ traps_test + 0x264 ]

     Source : <0x008f84ea> [ traps_test + 0x4aa ] CALL (P2)

   7 Target : <0x008f84cc> [ traps_test + 0x48c ]

     Source : <0x008fa1ca> [ traps_test + 0x218a ] RTS

   8 Target : <0x008fa1c4> [ traps_test + 0x2184 ]

     Source : <0x008fa274> [ traps_test + 0x2234 ] JUMP.S

   9 Target : <0x008fa272> [ traps_test + 0x2232 ]

     Source : <0x008fa258> [ traps_test + 0x2218 ] IF !CC JUMP

  10 Target : <0x008fa254> [ traps_test + 0x2214 ]

     Source : <0x008fa55c> [ traps_test + 0x251c ] RTS

  11 Target : <0x008fa548> [ traps_test + 0x2508 ]

     Source : <0xffa00b22> { __common_int_entry + 0xca } RTI

  12 Target : <0xffa00ac0> { __common_int_entry + 0x68 }

     Source : <0xffa00ce4> { _evt_system_call + 0x64 } JUMP.S

  13 Target : <0xffa00ce4> { _evt_system_call + 0x64 }

     Source : <0xffa007f4> { _system_call + 0xb8 } RTS

  14 Target : <0xffa007f0> { _system_call + 0xb4 }

     Source : <0xffa007e0> { _system_call + 0xa4 } IF !CC JUMP

  15 Target : <0xffa007da> { _system_call + 0x9e }

     Source : <0xffa007ca> { _system_call + 0x8e } IF !CC JUMP

Userspace Stack

Stack info:

SP: [0x008ffea0] <0x008ffea0> [ traps_test + 0x7ea0 ]

FP: (0x008ffeb4)

Memory from 0x008ffea0 to 00900000

008ffea0:[00000001] 00000000  008fff1c  00000000  00000000

(008fff1c)<008f84ec> 00000000

008ffec0: 00000013  0000002d  008fe1d0  00008a3b  081c0300  01000415  1a131100

170f1200

008ffee0: 00000016  00000000  00000000  00000000  00000000  00000000  008fffab

00000013

008fff00:<008fb140> 0000002f  008fff9d  008fff24 <008fc618>

008fc644  008fc644 (008fff38)

008fff20:<008fa49c> 00000000  008fe7c0  00000002  008fff7c  00000000

(00000000)<008c0598>

008fff40: 008fc644  008c6540  008c7f7c  00000000  008c67c0  00000002  008c03b4

00000000

008fff60: 00000000  00000000  008fc60c  008fc61e  00000000  008c67c0  00000002

008fff9c

008fff80: 008fffa9  00000000  008fffac  008fffb3  008fffc1  008fffe4  00000000

72742f2e

008fffa0: 5f737061  74736574  00393100  454d4f48  53002f3d  4c4c4548  69622f3d

68732f6e

008fffc0: 54415000  622f3d48  2f3a6e69  2f727375  3a6e6962  6962732f  752f3a6e

732f7273

008fffe0: 006e6962  4d524554  6e696c3d  2e007875  6172742f  745f7370  00747365

00000000

00900000: 544c4662

Return addresses in stack:

   frame  1 : <0x008f84ec> [ traps_test + 0x4ac ]

    address : <0x008fb140> [ traps_test + 0x3100 ]

    address : <0x008fc618> [ traps_test + 0x45d8 ]

   frame  2 : <0x008fa49c> [ traps_test + 0x245c ]

   frame  3 : <0x008c0598> [ traps_test + 0x598 ]

FAIL (test failed, but not with the right signal)

        (We expected 11 'Segmentation fault' but instead we got 4 'Illegal

instruction')

                                                                              

                                                                          

root:/bin> cat /proc/cpuinfo

processor       : 0

vendor_id       : Analog Devices

cpu family      : 0x27de

model name      : ADSP-BF548 525(MHz CCLK) 131(MHz SCLK) (mpu off)

stepping        : 1

cpu MHz         : 525.000/131.250000

bogomips        : 1044.48

Calibration     : 522240000 loops

cache size      : 16 KB(L1 icache) 32 KB(L1 dcache-wt) 0 KB(L2 cache)

dbank-A/B       : cache/cache

icache setup    : 4 Sub-banks/4 Ways, 32 Lines/Way

dcache setup    : 2 Super-banks/4 Sub-banks/2 Ways, 64 Lines/Way

L2 SRAM         : 128KB

board name      : ADI BF548-EZKIT

board memory    : 65536 kB (0x00000000 -> 0x04000000)

kernel memory   : 63480 kB (0x00001000 -> 0x03dff000)

 

root:/bin> cat /proc/cplbinfo/cpu0/dcplb

DCPLBs are enabled: 0x100f

Index   Address         Data    Size    U/RD    U/WR    S/WR    Switch

0       0x00000000      00083   1K      N       N       N       N

1       0x00000000      3d09d   4M      Y       Y       Y       N

2       0x00400000      3d09d   4M      Y       Y       Y       N

3       0x00800000      3d09d   4M      Y       Y       Y       N

4       0xff800000      3009f   4M      Y       Y       Y       N

5       0x20c00000      3009d   4M      Y       Y       Y       Y

6       0x03d00000      2d09d   1M      Y       Y       Y       Y

7       0x03e00000      2009d   1M      Y       Y       Y       Y

8       0x03f00000      2009d   1M      Y       Y       Y       Y

9       0x03c00000      2d09d   1M      Y       Y       Y       Y

10      0x03800000      3d09d   4M      Y       Y       Y       Y

11      0x00c00000      3d09d   4M      Y       Y       Y       Y

12      0x24000000      3009d   4M      Y       Y       Y       Y

13      0x21000000      3009d   4M      Y       Y       Y       Y

14      0x20400000      3009d   4M      Y       Y       Y       Y

15      0x20800000      3009d   4M      Y       Y       Y       Y

root:/bin> cat /proc/cplbinfo/cpu0/icplb

ICPLBs are enabled: 0x7

Index   Address         Data    Size    U/RD    U/WR    S/WR    Switch

0       0x00000000      31205   4M      Y       N       N       N

1       0x00400000      31205   4M      Y       N       N       N

2       0x00800000      31205   4M      Y       N       N       N

3       0xffa00000      30007   4M      Y       N       N       N

4       0x00c00000      31205   4M      Y       N       N       Y

5       0x03d00000      21205   1M      Y       N       N       Y

6       0x00000000      00000   1K      N       N       N       Y

7       0x00000000      00000   1K      N       N       N       Y

8       0x00000000      00000   1K      N       N       N       Y

9       0x00000000      00000   1K      N       N       N       Y

10      0x00000000      00000   1K      N       N       N       Y

11      0x00000000      00000   1K      N       N       N       Y

12      0x00000000      00000   1K      N       N       N       Y

13      0x00000000      00000   1K      N       N       N       Y

14      0x00000000      00000   1K      N       N       N       Y

15      0x00000000      00000   1K      N       N       N       Y

root:/bin> version

kernel:    Linux release 2.6.28-ADI-2009R1-pre-svn6041, build #18 Mon Feb 2

04:17:55 GMT 2009

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-7697, build #198 Mon Feb 2 04:16:19 GMT 2009

 

--- Bernd Schmidt                                            2009-02-04 09:14:58

This appears to be with MPU off.  Is CONFIG_DEBUG_HUNT_FOR_ZERO set for both

kernels?

 

--- Mingquan Pan                                             2009-02-06 04:05:54

All the kernels are set CONFIG_DEBUG_HUNT_FOR_ZERO to yes. The config for linux

is the same which is attached.

 

CONFIG_DEBUG_HUNT_FOR_ZERO=y

CONFIG_DEBUG_BFIN_HWTRACE_ON=y

CONFIG_DEBUG_BFIN_HWTRACE_COMPRESSION_OFF=y

# CONFIG_DEBUG_BFIN_HWTRACE_COMPRESSION_ONE is not set

 

--- Bernd Schmidt                                            2009-02-09 11:01:11

Sorry.  It should be fixed now.

 

--- Mingquan Pan                                             2009-02-10 01:30:48

Yes, it passed on all of those machines. Close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.traps    application/octet-stream    34822    Mingquan Pan

Attachments

Outcomes