[#4710] kernel will crash when record and play in bf527-ezkit

Document created by Aaronwu Employee on Aug 30, 2013
Version 1Show Document
  • View in full screen mode

[#4710] kernel will crash when record and play in bf527-ezkit

Submitted By: Vivi Li

Open Date

2008-12-10 05:22:39     Close Date

2009-01-20 05:19:29

Priority:

High     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

Audio     Board:

EZKIT Lite

Processor:

BF527     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

toolchain4.1_2008-11-13

App binary format:

N/A     

Summary: kernel will crash when record and play in bf527-ezkit

Details:

 

In bf527-ezkit, kernel will crash when record and play.

 

--

Linux version 2.6.28-rc2-ADI-2009R1-pre-svn5849 (test@107-local) (gcc version 4.1.2 (ADI svn)) #8 W8

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00141f70

  rodata    = 0x00141f70-0x001a4d00

  bss       = 0x001a4d00-0x001b5784

  data      = 0x001b5784-0x001c8000

    stack   = 0x001c6000-0x001c8000

  init      = 0x001c8000-0x0049a000

  available = 0x0049a000-0x03eff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Reset caused by Software reset

Blackfin support (C) 2004-2008 Analog Devices, Inc.

Compiled for ADSP-BF527 Rev 0.0

ERROR: Not running on ADSP-BF527: unknown CPUID 0x27e0 Rev 0.0

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables for global access

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16001

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart1,57600 console=tty0 console=ttyf

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 59216k/65536k RAM, (2888k init code, 1283k kernel code, 537k data, 1024k dma, 584)

Calibrating delay loop... 1046.52 BogoMIPS (lpj=2093056)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

PDA for CPU0 reserved at 001a5c38

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

musb_hdrc: version 6.0, pio, host, debug=0

musb_hdrc: USB Host mode controller at ffc03800 using PIO, IRQ 59

musb_hdrc musb_hdrc.0: MUSB HDRC host driver

musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 115

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-t350mcqb: 320x240 24-bit RGB FrameBuffer initializing...

dma_alloc_init: dma_page @ 0x03a4f000 - 256 pages at 0x03f00000

bfin-otp: initialized

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART

brd: module loaded

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_d)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

m25p80 spi0.1: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x00000000-0x00040000 : "bootloader(spi)"

0x00040000-0x00200000 : "linux kernel(spi)"

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma c7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

usbcore: registered new interface driver usbhid

usbhid: v2.6:USB HID core driver

Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).

ASoC version 0.13.2

dma rx:3 tx:4, err irq:15, regs:ffc00800

ssm2602 Audio Codec 0.1<4>hid_zpff: Unknown symbol _input_ff_create_memless

asoc: SSM2602 <-> bf5xx-i2s mapping ok

ALSA device list:

  #0: bf5xx_ssm2602 (SSM2602)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2004-05-31 05:42:01 UTC (1085982121)

usb 1-1: new high speed USB device using musb_hdrc and address 2

usb 1-1: configuration #1 chosen from 1 choice

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf527-ezkit, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 2888k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.1 (2008-12-10 17:54:01 CST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/> PHY: 0:01 - Link is Up - 100/Full

root:/>

root:/> arecord -t wav -c 2 -f S16_LE -r 8000 -d 5 wav

Recording WAVE 'wav' : Signed 16 bit Little Endian, Rate 8000 Hz, Stereo

root:/> aplay wav

NULL pointer access

Kernel OOPS in progress

Deferred Exception context

CURRENT PROCESS:

COMM=aplay PID=238

CPU = 0

TEXT = 0x00310000-0x0031b9ac        DATA = 0x0029a9ac-0x0029b5a4

BSS = 0x0029b5a4-0x002a0000  USER-STACK = 0x002bfeb0

 

return address: [0x000ea364]; contents of:

0x000ea340:  04c3  3218  0167  6f86  ac9a  ac52  acd2  ae94

0x000ea350:  ac62  0c42  181a  0000  0000  6059  e515  001c

0x000ea360:  e418  001c [a2aa] b0f2  e3ff  9046  e42a  0012

0x000ea370:  e418  001c  6041  b0f2  e3ff  903e  bca3  6c86

 

SEQUENCER STATUS:               Not tainted

SEQSTAT: 00062027  IPEND: 8030  SYSCFG: 0006

  EXCAUSE   : 0x27

  physical IVG15 asserted : <0xffa00cf4> { _evt_system_call + 0x0 }

  logical irq   6 mapped  : <0xffa0032c> { _timer_interrupt + 0x0 }

  logical irq  13 mapped  : <0x00095580> { _bfin_t350mcqb_irq_error + 0x0 }

  logical irq  15 mapped  : <0x000ec058> { _err_handler + 0x0 }

  logical irq  21 mapped  : <0x000c3ff4> { _bfin_rtc_interrupt + 0x0 }

  logical irq  23 mapped  : <0x000eae38> { _rx_handler + 0x0 }

  logical irq  24 mapped  : <0x000eadd4> { _tx_handler + 0x0 }

  logical irq  27 mapped  : <0x000c66a0> { _bfin_twi_interrupt_entry + 0x0 }

  logical irq  31 mapped  : <0x000a0f7c> { _bfin_serial_dma_rx_int + 0x0 }

  logical irq  32 mapped  : <0x000a127c> { _bfin_serial_dma_tx_int + 0x0 }

  logical irq  35 mapped  : <0x000a9234> { _bfin_mac_interrupt + 0x0 }

  logical irq  59 mapped  : <0x000bdbd4> { _blackfin_interrupt + 0x0 }

RETE: <0x00000000> { _do_one_initcall + 0xfffff000 }

RETN: <0x0023bce0> /* kernel dynamic memory */

RETX: <0x00000480> /* Maybe fixed code section */

RETS: <0x000e7d14> { _soc_pcm_open + 0x60 }

PC  : <0x000ea364> { _ssm2602_startup + 0x24 }

DCPLB_FAULT_ADDR: <0x00000028> /* Maybe null pointer? */

ICPLB_FAULT_ADDR: <0x000ea364> { _ssm2602_startup + 0x24 }

 

PROCESSOR STATE:

R0 : 03a63400    R1 : 0000000b    R2 : 00000000    R3 : 00000000

R4 : 001c08cc    R5 : 001c07b8    R6 : 001c094c    R7 : 00000000

P0 : 03a635f4    P1 : 00000140    P2 : 03a55aa0    P3 : 03a55ba0

P4 : 03a5ea20    P5 : 00000000    FP : 03a55ba0    SP : 0023bc04

LB0: 0008c2fa    LT0: 0008c2fa    LC0: 00000000

LB1: 0003bac2    LT1: 0003babc    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 03e79009

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 03bf5c00

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 0000003a   A0.x: 00000000   A1.w: 0000003a   A1.x: 00000000

USP : 002bf7cc  ASTAT: 02003005

 

Hardware Trace:

   0 Target : <0x000049f4> { _trap_c + 0x0 }

     Source : <0xffa00662> { _exception_to_level5 + 0x9e } CALL pcrel

   1 Target : <0xffa005c4> { _exception_to_level5 + 0x0 }

     Source : <0xffa0045a> { _bfin_return_from_exception + 0x6 } RTX

   2 Target : <0xffa00454> { _bfin_return_from_exception + 0x0 }

     Source : <0xffa0051e> { _ex_trap_c + 0x66 } JUMP.S

   3 Target : <0xffa004b8> { _ex_trap_c + 0x0 }

     Source : <0xffa006ee> { _trap + 0x2a } JUMP (P4)

   4 Target : <0xffa006c4> { _trap + 0x0 }

     Source : <0x000ea360> { _ssm2602_startup + 0x20 } 0xe418

   5 Target : <0x000ea340> { _ssm2602_startup + 0x0 }

     Source : <0x000e7d12> { _soc_pcm_open + 0x5e } CALL (P2)

   6 Target : <0x000e7cfe> { _soc_pcm_open + 0x4a }

     Source : <0x000ea906> { _bf5xx_pcm_open + 0x3e } RTS

   7 Target : <0x000ea8e8> { _bf5xx_pcm_open + 0x20 }

     Source : <0x000dd916> { _snd_pcm_hw_constraint_integer + 0x2e } RTS

   8 Target : <0x000dd8e8> { _snd_pcm_hw_constraint_integer + 0x0 }

     Source : <0x000ea8e4> { _bf5xx_pcm_open + 0x1c } CALL pcrel

   9 Target : <0x000ea8e0> { _bf5xx_pcm_open + 0x18 }

     Source : <0x000e707c> { _snd_soc_set_runtime_hwparams + 0x40 } RTS

  10 Target : <0x000e703c> { _snd_soc_set_runtime_hwparams + 0x0 }

     Source : <0x000ea8dc> { _bf5xx_pcm_open + 0x14 } CALL pcrel

  11 Target : <0x000ea8c8> { _bf5xx_pcm_open + 0x0 }

     Source : <0x000e7cfc> { _soc_pcm_open + 0x48 } CALL (P2)

  12 Target : <0x000e7ce6> { _soc_pcm_open + 0x32 }

     Source : <0x000ec3f4> { _bf5xx_i2s_startup + 0x10 } RTS

  13 Target : <0x000ec3e4> { _bf5xx_i2s_startup + 0x0 }

     Source : <0x000e7ce4> { _soc_pcm_open + 0x30 } CALL (P2)

  14 Target : <0x000e7cdc> { _soc_pcm_open + 0x28 }

     Source : <0x0014113a> { _mutex_lock + 0x32 } RTS

  15 Target : <0x00141114> { _mutex_lock + 0xc }

     Source : <0x00140b42> { __cond_resched + 0x1a } RTS

 

Kernel Stack

Stack info:

SP: [0x0023bf24] <0x0023bf24> /* kernel dynamic memory */

Memory from 0x0023bf20 to 0023c000

0023bf20: 002bf94c [0040d52a] 00008000  00002000  00000000  0023c000  0040d52a  0040d52a

0023bf40:<00268cf6><ffa00d58><02002020> 0041d7fb  004863d1  0041d7fa  004863c4  00000000

0023bf60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

0023bf80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

0023bfa0: 00000000  00000000  00000000  00436b40  00436b14  002bf7cc  002bf7dc  00000000

0023bfc0: ffffffff  00304df8  0030cbe0  0040d510  00000005  0030d4e0  00000802  002bf94c

0023bfe0: 00000001  002bf94c  00000000  00000802  002bf94c  002bf94c  00000005  00000006

0023c000: 00000000

Return addresses in stack:

    address : <0x00268cf6> [ /lib/libpthread-0.9.29.so + 0x8cf6 ]

    address : <0xffa00d58> { _evt_system_call + 0x64 }

    address : <0x02002020> /* kernel dynamic memory */

Modules linked in:

Kernel panic - not syncing: Kernel exception

--

 

Follow-ups

 

--- Cliff Cai                                                2009-01-12 04:41:24

fixed now,Set constraint only if the value is not 0.

 

Cliff

 

--- Vivi Li                                                  2009-01-20 05:19:29

OK, close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes