[#4653] It fails to build kernel with audio ssm2602 in BF527-EZKIT in trunk

Document created by Aaronwu Employee on Aug 29, 2013
Version 1Show Document
  • View in full screen mode

[#4653] It fails to build kernel with audio ssm2602 in BF527-EZKIT in trunk

Submitted By: Vivi Li

Open Date

2008-11-19 02:48:20     Close Date

2008-12-04 01:40:59

Priority:

Medium     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

Make Errors     Board:

EZKIT Lite

Processor:

BF527     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Under Debugging

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1 2008_Nov_13

App binary format:

N/A     

Summary: It fails to build kernel with audio ssm2602 in BF527-EZKIT in trunk

Details:

 

Build kernel with audio ssm2602 on BF527-EZKIT, it fails at bf5xx-ac97-pcm.c.

It will both fail when audio ssm2602 is built-in mode or module.

Config files are attached.

 

Bellow is the log when audio ssm2602 is built-in mode:

--

  LD      .tmp_vmlinux1^M

sound/built-in.o: In function `bf5xx_mmap_copy':^M

sound/soc/blackfin/bf5xx-ac97-pcm.c:(.text+0x1a274): undefined reference to `bf5xx_pcm_to_ac97'^M

sound/soc/blackfin/bf5xx-ac97-pcm.c:(.text+0x1a2b2): undefined reference to `bf5xx_ac97_to_pcm'^M

make[1]: *** [.tmp_vmlinux1] Error 1^M

make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x'^M

make: *** [linux] Error 1^M

--

 

Bellow is the log when audio ssm2602 is module:

--

  SYSMAP  System.map^M

  SYSMAP  .tmp_System.map^M

  OBJCOPY arch/blackfin/boot/vmlinux.bin^M

  GZIP    arch/blackfin/boot/vmlinux.gz^M

  Building modules, stage 2.^M

  MODPOST 41 modules^M

ERROR: "bf5xx_pcm_to_ac97" [sound/soc/blackfin/snd-bf5xx-ac97.ko] undefined!^M

ERROR: "bf5xx_ac97_to_pcm" [sound/soc/blackfin/snd-bf5xx-ac97.ko] undefined!^M

make[2]: *** [__modpost] Error 1^M

make[1]: *** [modules] Error 2^M

make[1]: *** Waiting for unfinished jobs....^M

--

 

Follow-ups

 

--- Cliff Cai                                                2008-11-28 02:32:16

SSM2602 should have nothing to do with ac97,so selecting I2S relative stuff is

enough.

 

Cliff

 

--- Vivi Li                                                  2008-12-04 01:40:59

I changed the build scripts and it's ok now.

Close it.

Thanks!

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.audio_ssm2602.module    application/octet-stream    36748    Vivi Li

config.audio_ssm2602.built-in    application/octet-stream    36737    Vivi Li

Outcomes