[#4612] Build kgdb kernel failed in BF561-EZKIT

Document created by Aaronwu Employee on Aug 29, 2013
Version 1Show Document
  • View in full screen mode

[#4612] Build kgdb kernel failed in BF561-EZKIT

Submitted By: Vivi Li

Open Date

2008-11-06 02:57:16     Close Date

2008-11-10 23:28:34

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Duplicate

Uboot version or rev.:

    Toolchain version or rev.:

toolchain-2008_Oct_10

App binary format:

N/A     

Summary: Build kgdb kernel failed in BF561-EZKIT

Details:

 

Build kgdb kernel failed in BF561-EZKIT.

 

--

  CHK     include/linux/compile.h^M

  UPD     include/linux/compile.h^M

  CC      init/version.o^M

  LD      init/built-in.o^M

  LD      .tmp_vmlinux1^M

arch/blackfin/kernel/built-in.o: In function `test_proc_output':^M

arch/blackfin/kernel/kgdb_test.c:88: relocation truncated to fit: R_pcrel24 against symbol `kgdb_l2_test' defined in .l2.text section in arch/blackfin/kernel/built-in.o^M

arch/blackfin/kernel/built-in.o: In function `kgdb_l2_test':^M

arch/blackfin/kernel/kgdb_test.c:67: relocation truncated to fit: R_pcrel24 against symbol `printk' defined in .text section in kernel/built-in.o^M

arch/blackfin/kernel/kgdb_test.c:68: relocation truncated to fit: R_pcrel24 against symbol `printk' defined in .text section in kernel/built-in.o^M

arch/blackfin/kernel/kgdb_test.c:70: relocation truncated to fit: R_pcrel24_jump_l against symbol `printk' defined in .text section in kernel/built-in.o^M

make[1]: *** [.tmp_vmlinux1] Error 1^M

make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x'^M

make: *** [linux] Error 1^M

--

 

Follow-ups

 

--- Sonic Zhang                                              2008-11-10 23:28:34

This is a duplicated bug of 4562.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes