[#4571] lmbench test case fails on bf527 ezkit board

Document created by Aaronwu Employee on Aug 29, 2013
Version 1Show Document
  • View in full screen mode

[#4571] lmbench test case fails on bf527 ezkit board

Submitted By: Mingquan Pan

Open Date

2008-10-29 03:43:29     Close Date

2008-12-03 04:09:10

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Duplicate

Uboot version or rev.:

    Toolchain version or rev.:

Sep 23

App binary format:

N/A     

Summary: lmbench test case fails on bf527 ezkit board

Details:

 

lmbench test case fails on bf527 ezkit board now, it didn't show the expected performance value when calling as :./lat_ctx -s 64 8, missing the numbers that should be on the second line.

 

get:

 

mbench3/bin/blackfin-Linux> ./lat_ctx -s 16 8^M

^M

"size=16k ovr=51.85^M

8 164.58^M

root:/lmbench3

Case 4 ...PASS

 

Case 4 ...PASS

/bin/blackfin-Linux> ./lat_ctx -s 64 8^M

^M

"size=64k ovr=630.86^M

root:/lmbench3/bin/blackfin-Linux>

Case 5 ...FAIL

 

It looks ok on other boards and this bug was first seen at about Sep 24.

 

Follow-ups

 

--- Sonic Zhang                                              2008-11-13 05:08:44

Can't replicate on SVN 5692

 

--- Mingquan Pan                                             2008-12-03 04:09:10

It is not happening every time, and on regression test machine, I still can see

this error show up from time to time.

 

Loading .text @ 0x00001000 (1189104 bytes)

Loading .rodata @ 0x001234f0 (296948 bytes)

Loading .init.rodata @ 0x0016bce4 (156 bytes)

Loading __ksymtab @ 0x0016bd80 (16680 bytes)

Loading __ksymtab_gpl @ 0x0016fea8 (5752 bytes)

Loading __ksymtab_strings @ 0x00171520 (50400 bytes)

Loading __init_rodata @ 0x0017da00 (172 bytes)

Loading __param @ 0x0017daac (640 bytes)

Clearing .bss @ 0x0017dd30 (66476 bytes)

Loading .data @ 0x0018e0dc (73508 bytes)

Loading .init.text @ 0x001a0000 (101488 bytes)

Loading .init.data @ 0x001b8c70 (20648 bytes)

Loading .init.setup @ 0x001bdd18 (584 bytes)

Loading .initcall.init @ 0x001bdf60 (644 bytes)

Loading .con_initcall.init @ 0x001be1e4 (4 bytes)

Loading .init.ramfs @ 0x001be1e8 (5293832 bytes)

Loading .text_l1 @ 0xffa00000 (5500 bytes)

sh_addr: FFA00000, p_paddr: 006CA8F0

Loading from: 026BB000 to 006CA8F0, size: 5500

Loading .data_l1 @ 0xff800000 (192 bytes)

sh_addr: FF800000, p_paddr: 006CBE6C

Loading from: 026BD000 to 006CBE6C, size: 192

## Starting application at 0x001ad480 ...

Linux version 2.6.28-rc2-ADI-2009R1-pre-svn5790 (test@uclinux60-bf527-std) (gcc

version 4.1.2 (ADI svn)) #49 Wed Dec 3 14:58:15 CST 2008

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001234f0

  rodata    = 0x001234f0-0x0017dd2c

  bss       = 0x0017dd30-0x0018e0dc

  data      = 0x0018e0dc-0x001a0000

    stack   = 0x0019e000-0x001a0000

  init      = 0x001a0000-0x006cc000

  available = 0x006cc000-0x03eff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Reset caused by Software reset

Blackfin support (C) 2004-2008 Analog Devices, Inc.

Compiled for ADSP-BF527 Rev 0.0

ERROR: Not running on ADSP-BF527: unknown CPUID 0x27e0 Rev 0.0

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables for global access

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16001

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600

ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:bf527-ezkit:eth0:off

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 56968k/65536k RAM, (5296k init code, 1161k kernel code, 499k

data, 1024k dma, 584k reserved)

Calibrating delay loop... 1044.48 BogoMIPS (lpj=2088960)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

PDA for CPU0 reserved at 0017ed68

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

musb_hdrc: version 6.0, pio, host, debug=0

musb_hdrc: USB Host mode controller at ffc03800 using PIO, IRQ 59

musb_hdrc musb_hdrc.0: MUSB HDRC host driver

musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 111

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-t350mcqb: 320x240 24-bit RGB FrameBuffer initializing...

dma_alloc_init: dma_page @ 0x0357f000 - 256 pages at 0x03f00000

bfin-otp: initialized

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART

brd: module loaded

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:03, irq=-1,

mdc_clk=2500000Hz(mdc_div=25)@sclk=131MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

m25p80 spi0.1: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x00000000-0x00040000 : "bootloader(spi)"

0x00040000-0x00200000 : "linux kernel(spi)"

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0,

regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

hid_tmff: Unknown symbol _input_ff_create_memless

usbcore: registered new interface driver usbhid

usbhid: v2.6:USB HID core driver

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2004-05-31 08:15:52 UTC

(1085991352)

usb 1-1: new high speed USB device using musb_hdrc and address 2

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf527-ezkit, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 5296k freed

usb 1-1: configuration #1 chosen from 1 choice

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.1 (2008-12-03 04:47:44 CST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/>

************** STEP 3: Start testing.

 

PHY: 0:03 - Link is Up - 100/Full

 

root:/> cd lmbench3/bin/blackfin-Linux

root:/lmbench3/bin/blackfin-Linux> ./lat_ctx -s 0 2

 

"size=0k ovr=17.05

2 34.99

root:/lmbench3/bin/blac

Case 1 ...PASS

 

Case 1 ...PASS

kfin-Linux> ./lat_ctx -s 16 2

 

"size=16k ovr=48.52

2 172.27

root:/lmbench3

Case 2 ...PASS

 

Case 2 ...PASS

/bin/blackfin-Linux> ./lat_ctx -s 64 2

 

"size=64k ovr=631.70

root:/lmbench3/bin/blackfin-Linux>

Case 3 ...FAIL

 

Case 3 ...FAIL

 

LMBENCH TEST FAIL

 

And this issue happens every time to Bf548 ezkit board logged in bug [#3965]

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes