[#4559] SMP patched kernel build faild with SMP disabled

Document created by Aaronwu Employee on Aug 29, 2013
Version 1Show Document
  • View in full screen mode

[#4559] SMP patched kernel build faild with SMP disabled

Submitted By: Graf Yang

Open Date

2008-10-21 22:06:36     Close Date

2008-11-14 06:20:51

Priority:

Medium     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

App binary format:

N/A     

Summary: SMP patched kernel build faild with SMP disabled

Details:

 

  CC [M]  net/sunrpc/stats.o

  CC      net/sysctl_net.o

  CC [M]  net/sunrpc/sysctl.o

  LD      net/xfrm/built-in.o

  LD [M]  net/sunrpc/sunrpc.o

  LD      net/built-in.o

  LD      vmlinux.o

  MODPOST vmlinux.o

  GEN     .version

  CHK     include/linux/compile.h

  UPD     include/linux/compile.h

  CC      init/version.o

  LD      init/built-in.o

  LD      .tmp_vmlinux1

init/built-in.o:在函数‘kernel_init’中:

init/main.c:(.init.text+0x4d6):对‘irq_flags’未定义的引用

init/main.c:(.init.text+0x4da):对‘irq_flags’未定义的引用

init/built-in.o:在函数‘start_kernel’中:

(.init.text+0x642):对‘irq_flags’未定义的引用

init/built-in.o:在函数‘start_kernel’中:

(.init.text+0x646):对‘irq_flags’未定义的引用

init/built-in.o:在函数‘start_kernel’中:

(.init.text+0x664):对‘irq_flags’未定义的引用

init/built-in.o:(.init.text+0x668): more undefined references to `irq_flags' follow

make[1]: *** [.tmp_vmlinux1] 错误 1

make[1]: Leaving directory `/opt/bfin/uclinux-dist/linux-2.6.x'

make: *** [linux] 错误 1

 

Follow-ups

 

--- Graf Yang                                                2008-10-23 03:53:07

It's a mistake in condition compile macros. Now should be fixed.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes