[#4551] kernel build with write back policy fails to be booted up now

Document created by Aaronwu Employee on Aug 29, 2013
Version 1Show Document
  • View in full screen mode

[#4551] kernel build with write back policy fails to be booted up now

Submitted By: Mingquan Pan

Open Date

2008-10-20 06:29:02     Close Date

2008-10-21 00:04:53

Priority:

Medium     Assignee:

Mike Frysinger

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

Oct 10

App binary format:

N/A     

Summary: kernel build with write back policy fails to be booted up now

Details:

 

kernel build with write back policy fails to be booted up from about Oct 15 on both BF533 STAMP and BF537-STAMP.

 

It stops at :

## Starting application at 0x001882a0 ...

Linux version 2.6.26.5-ADI-2009R1-pre-svn5444 (test@uclinux73-bf537-stamp-wb) (gcc version 4.1.2 (ADI svn)) #199 Mon Oct 20 18:22:06 CST 2008

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00108d00

  rodata    = 0x00108d00-0x0015a764

  bss       = 0x0015a780-0x00168ad8

  data      = 0x00168ad8-0x0017a000

    stack   = 0x00178000-0x0017a000

  init      = 0x0017a000-0x004fa000

  available = 0x004fa000-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Reset caused by Software reset

Blackfin support (C) 2004-2008 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Warning: Unsupported Chip Revision ADSP-BF537 Rev 0.2 detected

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 100 MHz System Clock

NOMPU: setting up cplb tables for global access

Instruction Cache Enabled

Data Cache Enabled (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600

Configuring Blackfin Priority Driven Interrupts

...

brd: module loaded

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=19)@sclk=100MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

bfin-spi bfin-spi.0: Blackfin BF5xx on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 00:07:19 UTC (439)

Freeing unused kernel memory: 3584k freed

dma_alloc_init: dma_page @ 0x004f6000 - 256 pages at 0x03f00000

 

No prompt shows up.

 

And if changes back to write through policy, it boots ok.

 

Follow-ups

 

--- Mike Frysinger                                           2008-10-20 10:07:07

i think i know what this is ...

 

--- Mike Frysinger                                           2008-10-20 15:34:27

the dcache/icache function that only gets used in writeback mode was putting

IFLUSH as the last instruction in the hardware loop ... we know from design that

this may often lead to inifite core stalling, so switch the FLUSH/IFLUSH order

 

should be fixed in trunk now

 

--- Mingquan Pan                                             2008-10-21 00:04:53

Yes,close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes