[#4469] Build kernel failed when SND_BF5XX_AC97 is enabled as module: undefined bf5xx_pcm_to_ac97 and bf5xx_ac97_to_pcm

Document created by Aaronwu Employee on Aug 29, 2013
Version 1Show Document
  • View in full screen mode

[#4469] Build kernel failed when SND_BF5XX_AC97 is enabled as module: undefined bf5xx_pcm_to_ac97 and bf5xx_ac97_to_pcm

Submitted By: Vivi Li

Open Date

2008-10-09 06:27:04     Close Date

2008-11-03 21:55:12

Priority:

Medium     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

toolchain Sep. 23

App binary format:

N/A     

Summary: Build kernel failed when SND_BF5XX_AC97 is enabled as module: undefined bf5xx_pcm_to_ac97 and bf5xx_ac97_to_pcm

Details:

 

Build kernel failed when SND_BF5XX_AC97 is enabled as module.

Attached is the config file. Bellow is the log.

 

--

  MODPOST vmlinux.o

  GEN     .version

  CHK     include/linux/compile.h

  UPD     include/linux/compile.h

  CC      init/version.o

  LD      init/built-in.o

  LD      .tmp_vmlinux1

  KSYM    .tmp_kallsyms1.S

  AS      .tmp_kallsyms1.o

  LD      .tmp_vmlinux2

  KSYM    .tmp_kallsyms2.S

  AS      .tmp_kallsyms2.o

  LD      vmlinux

  SYSMAP  System.map

  SYSMAP  .tmp_System.map

  OBJCOPY arch/blackfin/boot/vmlinux.bin

  GZIP    arch/blackfin/boot/vmlinux.gz

  Building modules, stage 2.

  MODPOST 62 modules

ERROR: "bf5xx_pcm_to_ac97" [sound/soc/blackfin/snd-bf5xx-ac97.ko] undefined!

ERROR: "bf5xx_ac97_to_pcm" [sound/soc/blackfin/snd-bf5xx-ac97.ko] undefined!

make[2]: *** [__modpost] Error 1

make[1]: *** [modules] Error 2

--

 

Follow-ups

 

--- Cliff Cai                                                2008-10-31 05:12:22

it's ok on latest trunk now

 

--- Vivi Li                                                  2008-11-03 21:50:12

OK now. Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.ac97    application/octet-stream    31540    Vivi Li

Attachments

Outcomes