[#4468] Build kernel failed when SND_BF5XX_I2S and SND_BF5XX_AC97 are enabled as built-in mode

Document created by Aaronwu Employee on Aug 29, 2013
Version 1Show Document
  • View in full screen mode

[#4468] Build kernel failed when SND_BF5XX_I2S and SND_BF5XX_AC97 are enabled as built-in mode

Submitted By: Vivi Li

Open Date

2008-10-09 06:01:35     Close Date

2008-11-03 21:54:44

Priority:

Medium     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

toolchain Sep. 23

App binary format:

N/A     

Summary: Build kernel failed when SND_BF5XX_I2S and SND_BF5XX_AC97 are enabled as built-in mode

Details:

 

Build kernel failed when SND_BF5XX_I2S and SND_BF5XX_AC97 are enabled as built-in mode.

Bellow is the log and config file is attached.

 

--

  CC      sound/soc/blackfin/bf5xx-ssm2602.o^M

  CC      drivers/rtc/class.o^M

  LD      sound/soc/blackfin/snd-bf5xx-ac97.o^M

  LD      sound/soc/blackfin/snd-bf5xx-i2s.o^M

  LD      sound/soc/blackfin/snd-soc-bf5xx-sport.o^M

  LD      sound/soc/blackfin/snd-soc-bf5xx-i2s.o^M

  LD      sound/soc/blackfin/snd-ssm2602.o^M

  LD      sound/soc/blackfin/built-in.o^M

  CC      drivers/rtc/interface.o^M

sound/soc/blackfin/snd-bf5xx-i2s.o:(.data+0x0): multiple definition of `bf5xx_pcm_ops'^M

sound/soc/blackfin/snd-bf5xx-ac97.o:(.data+0x0): first defined here^M

sound/soc/blackfin/snd-bf5xx-i2s.o: In function `bf5xx_pcm_new':^M

(.text+0x2a0): multiple definition of `bf5xx_pcm_new'^M

sound/soc/blackfin/snd-bf5xx-ac97.o:(.text+0x534): first defined here^M

make[4]: *** [sound/soc/blackfin/built-in.o] Error 1^M

--

 

Follow-ups

 

--- Cliff Cai                                                2008-10-31 05:13:16

it's OK on latest trunk now

 

--- Vivi Li                                                  2008-11-03 21:54:44

OK now. Close it.

Thanks!

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.audio_ad1981b    application/octet-stream    31408    Vivi Li

Attachments

Outcomes