[#4446] gptimer0 is the only one disabled whatever is the PPI port configuration

Document created by Aaronwu Employee on Aug 29, 2013
Version 1Show Document
  • View in full screen mode

[#4446] gptimer0 is the only one disabled whatever is the PPI port configuration

Submitted By: Jean-Francois Argentino

Open Date

2008-09-26 09:54:45     Close Date

2008-10-20 04:36:13

Priority:

Medium     Assignee:

Michael Hennerich

Status:

Closed     Fixed In Release:

N/A

Found In Release:

snaps     Release:

Category:

Drivers     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Assigned (Not Start)

Uboot version or rev.:

    Toolchain version or rev.:

SVN

App binary format:

N/A     

Summary: gptimer0 is the only one disabled whatever is the PPI port configuration

Details:

 

In the SVN version of bfin_ppi.c driver, I think there's a problem for disabling multiplexed GP TIMER, since evaluation of line 678 always return 0, then only GP timer 0 output is disabled, even if PPI is configured with 2 external frame synchronization signals.

Attached a patch to correct it.

 

Follow-ups

 

--- Michael Hennerich                                        2008-10-20 04:36:13

Patch applied on svn trunk and 2008R1 branch

Thanks for contributing

 

-Michael

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

ppi_patch_1    application/octet-stream    645    Jean-Francois Argentino

Attachments

Outcomes