[#4414] kernel build with config kernel debugging with remote gdb fails on trunk

Document created by Aaronwu Employee on Aug 29, 2013
Version 1Show Document
  • View in full screen mode

[#4414] kernel build with config kernel debugging with remote gdb fails on trunk

Submitted By: Mingquan Pan

Open Date

2008-09-10 22:37:47     Close Date

2008-09-19 06:53:04

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

Sep 08 toolchain

App binary format:

N/A     

Summary: kernel build with config kernel debugging with remote gdb fails on trunk

Details:

 

kernel build with this config KGDB: kernel debugging with remote gdb fails on trunk.

 

  CC      init/do_mounts_initrd.o

  CC      init/initramfs.o

  CC      init/calibrate.o

  CC      init/version.o

  LD      init/mounts.o

  LD      init/built-in.o

  GEN     usr/initramfs_data.cpio.gz

  AS      usr/initramfs_data.o

  LD      usr/built-in.o

  AS      arch/blackfin/kernel/entry.o

  CC      arch/blackfin/kernel/process.o

  CC      arch/blackfin/kernel/bfin_ksyms.o

  CC      arch/blackfin/kernel/ptrace.o

  CC      arch/blackfin/kernel/setup.o

  CC      arch/blackfin/kernel/signal.o

  CC      arch/blackfin/kernel/sys_bfin.o

  CC      arch/blackfin/kernel/traps.o

arch/blackfin/kernel/traps.c: In function 鈥榯rap_c鈥�

arch/blackfin/kernel/traps.c:320: error: duplicate case value

arch/blackfin/kernel/traps.c:289: error: previously used here

make[2]: *** [arch/blackfin/kernel/traps.o] Error 1

make[1]: *** [arch/blackfin/kernel] Error 2

make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x'

make: *** [linux] Error 1

 

Follow-ups

 

--- Sonic Zhang                                              2008-09-17 06:32:07

Fixed.

 

--- Mingquan Pan                                             2008-09-19 06:53:04

Yes,close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes