[#4391] some characters are missing when catted to host ttyUSB0 through UART1 on bf537 stamp

Document created by Aaronwu Employee on Aug 29, 2013
Version 1Show Document
  • View in full screen mode

[#4391] some characters are missing when catted to host ttyUSB0 through UART1 on bf537 stamp

Submitted By: Mingquan Pan

Open Date

2008-08-27 05:08:23     Close Date

2008-12-03 03:55:25

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Not reproducible

Uboot version or rev.:

    Toolchain version or rev.:

trunk head toolchain

App binary format:

N/A     

Summary: some characters are missing when catted to host ttyUSB0 through UART1 on bf537 stamp

Details:

 

some characters are missing when catted to host ttyUSB0 through UART1 on bf537 stamp board.

 

When cat boa.conf to host /dev/ttyUSB0,some chars are cut,only get:

 

diff -u a boa.conf

--- a   2008-08-27 17:27:14.000000000 +0800

+++ boa.conf    2008-08-27 17:27:18.000000000 +0800

@@ -1,4 +1,4 @@

- Boa v0.94 configuration file

+# Boa v0.94 configuration file

# File format has changed little from 0.92

# version changes are noted in the comments

#

@@ -118,7 +118,7 @@

 

#CodepageByBrowser Lynx/* us-ascii

 

-# KeepAliveMax: Number of KeepAlive requests to a Boa v0.94 configuration file^llow per connection

+# KeepAliveMax: Number of KeepAlive requests to allow per connection

# Comment out, or set to 0 to disable keepalive processing

 

KeepAliveMax 1

 

The whole log is attached.

 

Follow-ups

 

--- Sonic Zhang                                              2008-09-25 04:09:03

Can't replicate.

 

--- Mingquan Pan                                             2008-12-03 03:55:25

It is fine on trunk now.Close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

serial_uart1_test_log    application/octet-stream    18062    Mingquan Pan

Attachments

Outcomes