[#4365] Warning when building SPI_MMC in svn trunk 2.6.26

Document created by Aaronwu Employee on Aug 29, 2013
Version 1Show Document
  • View in full screen mode

[#4365] Warning when building SPI_MMC in svn trunk 2.6.26

Submitted By: Bryan Wu

Open Date

2008-08-14 07:30:25     Close Date

2008-08-15 09:44:50

Priority:

Medium     Assignee:

Bryan Wu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

App binary format:

N/A     

Summary: Warning when building SPI_MMC in svn trunk 2.6.26

Details:

 

  CC      drivers/mmc/spi_mmc/bfin_pio_spi.o

drivers/mmc/spi_mmc/bfin_pio_spi.c:8:1: warning: "SPI0_REGBASE" redefined

In file included from include/asm/mach/blackfin.h:39,

                 from include/asm/blackfin.h:89,

                 from include/asm/system.h:208,

                 from include/asm/bitops.h:10,

                 from include/linux/bitops.h:17,

                 from include/linux/kernel.h:15,

                 from drivers/mmc/spi_mmc/bfin_pio_spi.c:1:

include/asm/mach/defBF534.h:89:1: warning: this is the location of the previous definition

 

Follow-ups

 

--- Bryan Wu                                                 2008-08-14 07:32:11

Fixed in the trunk

 

-Bryan

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes