[#4249] LZO's configure uses _AC_SRCPATHS, not _AC_SRCDIRS

Document created by Aaronwu Employee on Aug 29, 2013
Version 1Show Document
  • View in full screen mode

[#4249] LZO's configure uses _AC_SRCPATHS, not _AC_SRCDIRS

Submitted By: David Gravereaux

Open Date

2008-07-16 21:15:54     Close Date

2008-07-18 04:04:59

Priority:

Medium     Assignee:

Mike Frysinger

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

svn up'd an hour ago

Category:

Make Errors     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

App binary format:

N/A     

Summary: LZO's configure uses _AC_SRCPATHS, not _AC_SRCDIRS

Details:

 

lzo fails to run configure with:

 

./configure: line 2150: syntax error near unexpected token `.'

./configure: line 2150: `    _AC_SRCPATHS(.)'

 

_AC_SRCPATHS not known to autoconf 2.61.  Should be _AC_SRCDIRS

 

 

patch:

davygrvy@techbench1:~/blackfin-sources/uclinux-dist/lib/lzo/lzo-2.02$ svn diff configure.ac

Index: configure.ac

===================================================================

--- configure.ac        (revision 6904)

+++ configure.ac        (working copy)

@@ -47,7 +47,7 @@

AM_MAINTAINER_MODE

 

if test -z "$ac_abs_top_srcdir"; then

-    _AC_SRCPATHS(.)

+    _AC_SRCDIRS(.)

fi

if test -r .Conf.settings1; then

     . ./.Conf.settings1

 

Follow-ups

 

--- Mike Frysinger                                           2008-07-16 21:30:25

that means autotools was run on your system when it should have not

 

i'm guessing you're using the branch and not the trunk, so i'll just add a

`find|touch` like normal

 

--- David Gravereaux                                         2008-07-16 21:54:18

yes, I traced it down to configure.in for you.  Apparently, 'configure' as

gotten from the trunk called it, but now that doesn't make sense...  No

scrollback left.. can't say for sure

 

--- Mike Frysinger                                           2008-07-18 04:04:58

right, but the configure script that exists in svn does not have _AC_SRCPATHS()

in it, and since autotools should not be run at all, your configure should not

end up with it in it.  we try to avoid touching upstream code where possible and

since there is no need for us to fix the configure.in otherwise, we'll let the

bug sit there.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes