[#4123] Fail to build qt source files in flat format

Document created by Aaronwu Employee on Aug 29, 2013
Version 1Show Document
  • View in full screen mode

[#4123] Fail to build qt source files in flat format

Submitted By: Vivi Li

Open Date

2008-05-22 23:14:44     Close Date

2008-06-04 22:43:56

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

08r1-rc8

App binary format:

N/A     

Summary: Fail to build qt source files in flat format

Details:

 

It failed to build qt source files in flat format.

 

Bellow is the error log. The full log is attached.

--

bfin-uclinux-g++ -c -pipe -D__linux__ -DQT_NO_LIBRARY -DQT_NOMMU -DQ_NO_SEMAPHORE -DQT_QWS_NO_SHM -DQT_NO_QWS_MULTIPROCESS -DQWS -fno-exceptions -fno-rtti -Wall -W -O2 -D_REENTRANT -DQT_NO_DEBUG -DQT_THREAD_SUPPORT -DQT_THREAD_SUPPORT -DQT_NO_CUPS -DQT_NO_NIS -DQT_NO_STYLE_MAC -DQT_NO_STYLE_AQUA -DQT_NO_STYLE_INTERLACE -DQT_NO_STYLE_WINDOWSXP -DQT_NO_STYLE_COMPACT -DQT_NO_STYLE_POCKETPC -DQT_NO_QWS_VFB -DQT_NO_QWS_VNC -DQT_NO_QWS_VGA16 -DQT_NO_QWS_TRANSFORMED -DQT_NO_QWS_SNAP -DQT_NO_QWS_MACH64 -DQT_NO_QWS_VOODOO3 -DQT_NO_QWS_MATROX -DQT_NO_QWS_SHADOWFB -DQT_NO_QWS_REPEATER -DQT_NO_QWS_KBD_SL5000 -DQT_NO_QWS_KBD_USB -DQT_NO_QWS_KBD_YOPY -DQT_NO_QWS_KBD_VR41 -DQT_NO_QWS_MOUSE_BUS -DQT_NO_QWS_MOUSE_LINUXTP -DQT_NO_QWS_MOUSE_VR41 -DQT_NO_QWS_MOUSE_YOPY -I/home/test/work/cruise/test_app/qt/qt-embedded-free-3.3.5/mkspecs/qws/linux-bfin-g++ -I. -I3rdparty/freetype/src -I3rdparty/freetype/include -I3rdparty/freetype/builds/unix -I3rdparty/freetype2/include -I3rdparty/libmng -I3rdparty/libjpeg -I3rdparty/libpng -I3rdparty/zlib -I../include -I.moc/release-static-mt-emb-bfin/ -o .obj/release-static-mt-emb-bfin/qeventloop_qws.o kernel/qeventloop_qws.cpp^M

In file included from kernel/qeventloop_p.h:47,^M

                 from kernel/qeventloop_qws.cpp:31:^M

/home/test/work/cruise/test_app/qt/qt-embedded-free-3.3.5/mkspecs/qws/linux-bfin-g++/qplatformdefs.h:41:19: error: dlfcn.h: No such file or directory^M

kernel/qwindowsystem_qws.h:223: warning: ‘class QWSServer::KeyboardFilter’ has virtual functions non-virtual destructor^M

kernel/qeventloop_qws.cpp: In member function ‘virtual bool QEventLoop::processEvents(uint)’:^M

kernel/qeventloop_qws.cpp:269: warning: ‘ret’ may be used uninitialized in this function^M

make[2]: *** [.obj/release-static-mt-emb-bfin/qeventloop_qws.o] Error 1^M

make[2]: Leaving directory `/home/test/work/cruise/test_app/qt/qt-embedded-free-3.3.5/src'^M

make[1]: *** [sub-src] Error 2^M

make[1]: Leaving directory `/home/test/work/cruise/test_app/qt/qt-embedded-free-3.3.5'^M

make: *** [init] Error 2^M

test@linux-bf527-std:~/work/cruise/test_app/qt/qt-embedded-free-3.3.5>

--

 

Follow-ups

 

--- Sonic Zhang                                              2008-05-26 00:29:34

Fixed.

 

--- Vivi Li                                                  2008-06-04 22:43:55

OK now. Close it.

Thannks!

 

-Vivi

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

build_qt_source_log.flat    text/plain    2074864    Vivi Li

Outcomes