[#4116] Under run error occurs sometimes in BF548-EZKIT in trunk

Document created by Aaronwu Employee on Aug 29, 2013
Version 1Show Document
  • View in full screen mode

[#4116] Under run error occurs sometimes in BF548-EZKIT in trunk

Submitted By: Vivi Li

Open Date

2008-05-20 05:40:56     Close Date

2008-05-21 22:56:54

Priority:

Medium     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

08r1-rc8

App binary format:

N/A     

Summary: Under run error occurs sometimes in BF548-EZKIT in trunk

Details:

 

Under run error occurs sometimes in BF548-EZKIT with audio dirver AD1980.

It happens when record while play.

 

--

vrec -w -b 16 -s 11000 -t 8 aaa^M

Recording WAVE : 16 bit, Speed 11000 Hz Mono ...^M

root:/> vplay aaa &^M

Playing WAVE : 16 bit, Speed 11000 Hz Mono ...^M

295^M

root:/> ^M

root:/> vrec -w -b 16 -s 11000 -t 4 bbb^M

Recording WAVE sp16oritt Spstd at00usHz eonrr..or

: TUVF^M

root:/>

--

 

Follow-ups

 

--- Vivi Li                                                  2008-05-21 22:56:51

Here is a workaround: set DMA to higer priority over core when build kernel.

Close this bug.

 

--- Robin Getz                                               2008-05-22 10:50:05

Vivi:

 

Which setting are you changing?

 

If a default setting needs to be changed, we should change it in the default

settings in svn - not in a test script.

 

-Robin

 

--- Cliff Cai                                                2008-05-22 22:37:38

This is a global setting,it will affect core's perfomance.

So,I think it's better to set it only if need. 

 

Cliff

 

--- Robin Getz                                               2008-05-23 21:23:14

People can unset it as easy as they can set it.

 

I would rather the default config have audio working robustly.

 

-Robin

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes