[#4058] i2ctwi BFIN_TWIKEYPAD_IRQ_PFX has no value for bf527 ezkit on 08r1

Document created by Aaronwu Employee on Aug 28, 2013
Version 1Show Document
  • View in full screen mode

[#4058] i2ctwi BFIN_TWIKEYPAD_IRQ_PFX has no value for bf527 ezkit on 08r1

Submitted By: Mingquan Pan

Open Date

2008-04-24 05:06:36     Close Date

2008-05-07 03:08:06

Priority:

Medium     Assignee:

Bryan Wu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

08r1-8

App binary format:

N/A     

Summary: i2ctwi BFIN_TWIKEYPAD_IRQ_PFX has no value for bf527 ezkit on 08r1

Details:

 

i2ctwi BFIN_TWIKEYPAD_IRQ_PFX has no value for bf527 ezkit on 08r1.

 

In linux-2.6.x/drivers/input/misc/Kconfig of 08r1, there is:

 

config BFIN_TWIKEYPAD_IRQ_PFX

        int "IRQ"

        depends on (BLACKFIN && TWI_KEYPAD)

        default "72" if BFIN537_STAMP

        default "39" if BFIN533_STAMP

        default "212" if BFIN548_EZKIT

        help

          Choose an GPIO as Keypad interrupt [33..120]

 

No value set to BFIN527_EZKIT.

 

 

 

Follow-ups

 

--- Bryan Wu                                                 2008-04-30 03:11:14

It was fixed in trunk and 2008R1 branch.

 

-Bryan

 

--- Mingquan Pan                                             2008-05-07 03:08:06

Yed,close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes