[#4029] smb fails to mount for fork failure

Document created by Aaronwu Employee on Aug 28, 2013
Version 1Show Document
  • View in full screen mode

[#4029] smb fails to mount for fork failure

Submitted By: Mingquan Pan

Open Date

2008-04-14 03:45:56     Close Date

2008-04-15 02:14:45

Priority:

Medium     Assignee:

Mike Frysinger

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

08r1-rc8

App binary format:

N/A     

Summary: smb fails to mount for fork failure

Details:

 

smb fails to mount for fork failure from about April 10th.

 

bfin> bootelf

Loading .text @ 0x00001000 (1080976 bytes)

Loading .exit.text.refok @ 0x00108e90 (296 bytes)

Loading .rodata @ 0x00108fc0 (259856 bytes)

Loading __ksymtab @ 0x001486d0 (14960 bytes)

Loading __ksymtab_gpl @ 0x0014c140 (4168 bytes)

Loading __ksymtab_strings @ 0x0014d188 (45988 bytes)

Loading __param @ 0x0015852c (300 bytes)

Clearing .bss @ 0x00158660 (59748 bytes)

Loading .data @ 0x00166fc4 (77884 bytes)

Loading .init.text @ 0x0017a000 (98040 bytes)

Loading .init.data @ 0x00191ef8 (13180 bytes)

Loading .init.setup @ 0x00195274 (612 bytes)

Loading .initcall.init @ 0x001954d8 (452 bytes)

Loading .con_initcall.init @ 0x0019569c (4 bytes)

Loading .init.ramfs @ 0x001956a0 (3968420 bytes)

Loading .text_l1 @ 0xffa00000 (6984 bytes)

sh_addr: FFA00000, p_paddr: 0055E444

Loading from: 02551000 to 0055E444, size: 6984

Loading .data_l1 @ 0xff800000 (192 bytes)

sh_addr: FF800000, p_paddr: 0055FF8C

Loading from: 02553000 to 0055FF8C, size: 192

## Starting application at 0x0017a000 ...

Linux version 2.6.24.4-ADI-2008R2-pre-svn4591 (test@uclinux51-ad9960-ad1836) (gcc version 4.1.2 (ADI svn)) #49 Sat Apr 12 13:22:28 CST 2008

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00108e90

  rodata    = 0x00108fc0-0x00158658

  bss       = 0x00158660-0x00166fc4

  data      = 0x00166fc4-0x0017a000

    stack   = 0x00178000-0x0017a000

  init      = 0x0017a000-0x00561000

  available = 0x00561000-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Reset caused by Software reset

Blackfin support (C) 2004-2008 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 100 MHz System Clock

NOMPU: setting up cplb tables for global access

Instruction Cache Enabled

Data Cache Enabled (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14224

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 51252k/65536k RAM, (3996k init code, 1055k kernel code, 453k data, 1024k dma, 7756k reserved)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin Data A SRAM: 16 KB (15 KB free)

Blackfin Data B SRAM: 16 KB (16 KB free)

Blackfin Instruction SRAM: 48 KB (41 KB free)

Security Framework initialized

Mount-cache hash table entries: 512

net_namespace: 64 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

RAMDISK driver initialized: 16 RAM disks of 4096K size 1024 blocksize

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=19)@sclk=100MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

bfin-spi bfin-spi.0: Blackfin BF5xx on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 03:46:05 UTC (13565)

Freeing unused kernel memory: 3996k freed

dma_alloc_init: dma_page @ 0x0055e000 - 256 pages at 0x03f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.10.0 (2008-04-12 12:14:50 CST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/>

************** STEP 3: Start tetsting.

 

ifconfig eth0 10.100.4.50

root:/> PHY: 0:01 - Link is Up - 100/Full

ifconfig

eth0      Link encap:Ethernet  HWaddr F2:B2:84:D7:34:26

          inet addr:10.100.4.50  Bcast:10.255.255.255  Mask:255.0.0.0

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

 

lo        Link encap:Local Loopback

          inet addr:127.0.0.1  Mask:255.0.0.0

          UP LOOPBACK RUNNING  MTU:16436  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

 

root:/> smbmount //10.100.4.174/users /mnt rw -o username=test,password=test

params.c:OpenConfFile() - Unable to open configuration file "/etc/config/smb.conf":

        No such file or directory

Can't load /etc/config/smb.conf - run testparm to debug it

could not fork

waitpid failed: Error was No child processesroot:/> cp /bin/version /mnt/test

root:/>

 

Follow-ups

 

--- Mike Frysinger                                           2008-04-14 05:10:53

i'll take this

 

--- Mike Frysinger                                           2008-04-14 05:22:46

there was a typo in configure.in where it wouldnt save CPPFLAGS at the right

place and then later restore an unset var thus clobbering the CPPFLAGS value

 

--- Mingquan Pan                                             2008-04-15 00:22:11

Yes,the smb can fork now.

Unfortunately, the can't open file issue still remaining.

 

 

Now, the running log is:

 

root:/> smbmount //10.100.4.174/users /mnt rw -o

username=test,password=test

params.c:OpenConfFile() - Unable to open configuration file

"/etc/config/smb.conf":

        No such file or directory

Can't load /etc/config/smb.conf - run testparm to debug it

root:/> cp /bin/version /mnt/test

root:/>

 

Since it is shown in the above bug report, I would prefer continue with it

rather than file a new bug,unless you protest...:)

 

--- Mike Frysinger                                           2008-04-15 00:35:06

that's a warning, not an error ... are you saying the mount doesnt work for you

?

 

--- Mingquan Pan                                             2008-04-15 02:14:45

It can mount,and it can also find the config file now after your change in

Makefile.Close,

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes