[#4015] portmap needs to port to nommu too

Document created by Aaronwu Employee on Aug 28, 2013
Version 1Show Document
  • View in full screen mode

[#4015] portmap needs to port to nommu too

Submitted By: Mingquan Pan

Open Date

2008-04-07 04:14:47     Close Date

2009-03-02 05:28:22

Priority:

Medium     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2008R1.5-RC3     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

08r1-8

App binary format:

N/A     

Summary: portmap needs to port to nommu too

Details:

 

trunk portmap needs to port to nommu too.It also has  Function not implemented failure when executed.

 

The kernel info:

Linux version 2.6.24.3-ADI-2008R2-pre-svn4482 (test@uclinux51-ad9960-ad1836) (gcc version 4.1.2 (ADI svn)) #8 Mon Mar 24 23:24:41 CST 2008^

...

 

root:/> portmap &^M

portmap: fork: Function not implemented^M

128^M

ro

 

Follow-ups

 

--- Mike Frysinger                                           2008-04-07 04:20:22

just use the -f option in the meantime

 

--- Graf Yang                                                2008-04-17 08:31:42

As Mike have pointed out, we must use -f option to put it run on foreground.

Thus it will not call fork().

 

--- Graf Yang                                                2008-07-15 02:49:58

Could it be closed?

 

--- Mike Frysinger                                           2008-07-15 03:15:20

the question is whether to make the daemonize step work for no mmu, or just

force people to use -f

 

it doesnt particularly matter to me either way

 

--- Sonic Zhang                                              2008-07-15 22:20:11

-f is acceptable for NOMMU.

 

--- Jie Zhang                                                2009-06-01 03:29:04

I have committed a patch for portmap to enclose fork with NO_MMU macro.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes