[#3987] trunk kernel build fails at ide-blackfin.c

Document created by Aaronwu Employee on Aug 28, 2013
Version 1Show Document
  • View in full screen mode

[#3987] trunk kernel build fails at ide-blackfin.c

Submitted By: Mingquan Pan

Open Date

2008-03-26 06:03:58     Close Date

2008-04-01 16:59:05

Priority:

Medium     Assignee:

Michael Hennerich

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Assigned (Not Start)

Uboot version or rev.:

    Toolchain version or rev.:

08r1-8

App binary format:

N/A     

Summary: trunk kernel build fails at ide-blackfin.c

Details:

 

trunk kernel build fails at ide-blackfin.c on bf537 stamp now.

 

log is:

 

  LD      drivers/i2c/built-in.o^M

  CC [M]  drivers/i2c/i2c-core.o^M

  CC [M]  drivers/i2c/i2c-dev.o^M

  LD      drivers/ide/arm/built-in.o^M

  LD      drivers/ide/legacy/built-in.o^M

  LD      drivers/ide/mips/built-in.o^M

  LD      drivers/ide/pci/built-in.o^M

  CC      drivers/ide/ide.o^M

  CC      drivers/ide/ide-io.o^M

  CC      drivers/ide/ide-iops.o^M

drivers/ide/ide-iops.c: In function 鈥榠de_inb鈥�^M

drivers/ide/ide-iops.c:39: warning: passing argument 1 of 鈥榬eadb鈥�makes pointer from integer without a cast^M

drivers/ide/ide-iops.c: In function 鈥榠de_inw鈥�^M

drivers/ide/ide-iops.c:44: warning: passing argument 1 of 鈥榬eadw鈥�makes pointer from integer without a cast^M

  CC      drivers/ide/ide-lib.o^M

  CC      drivers/ide/ide-probe.o^M

  CC      drivers/ide/ide-taskfile.o^M

  CC      drivers/ide/ide-proc.o^M

  CC      drivers/ide/blackfin/ide-blackfin.o^M

drivers/ide/blackfin/ide-blackfin.c: In function 鈥榟w_setup鈥�^M

drivers/ide/blackfin/ide-blackfin.c:94: error: 鈥榟w_regs_t鈥�has no member named 鈥榙ma鈥^M

drivers/ide/blackfin/ide-blackfin.c:94: error: 鈥楴O_DMA鈥�undeclared (first use in this function)^M

drivers/ide/blackfin/ide-blackfin.c:94: error: (Each undeclared identifier is reported only once^M

drivers/ide/blackfin/ide-blackfin.c:94: error: for each function it appears in.)^M

drivers/ide/blackfin/ide-blackfin.c: In function 鈥榟wif_setup鈥�^M

drivers/ide/blackfin/ide-blackfin.c:107: warning: assignment from incompatible pointer type^M

drivers/ide/blackfin/ide-blackfin.c:108: warning: assignment from incompatible pointer type^M

drivers/ide/blackfin/ide-blackfin.c: In function 鈥榖lackfin_ide_init鈥�^M

drivers/ide/blackfin/ide-blackfin.c:131: warning: passing argument 2 of 鈥榠de_register_hw鈥�makes pointer from integer without a cast^M

drivers/ide/blackfin/ide-blackfin.c:131: warning: passing argument 3 of 鈥榠de_register_hw鈥�makes integer from pointer without a cast^M

drivers/ide/blackfin/ide-blackfin.c:131: error: too few arguments to function 鈥榠de_register_hw鈥^M

make[3]: *** [drivers/ide/blackfin/ide-blackfin.o] Error 1^M

make[2]: *** [drivers/ide] Error 2^M

make[1]: *** [drivers] Error 2^M

make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x'^M

make: *** [linux] Error 1^M

 

 

config file is attached.

 

 

Follow-ups

 

--- Mike Frysinger                                           2008-04-01 16:59:05

this driver has been punted now

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.ide_cdrom    application/octet-stream    30363    Mingquan Pan

Attachments

    Outcomes