[#3964] trunk kernel build joystick fails

Document created by Aaronwu Employee on Aug 28, 2013
Version 1Show Document
  • View in full screen mode

[#3964] trunk kernel build joystick fails

Submitted By: Mingquan Pan

Open Date

2008-03-12 06:16:17     Close Date

2008-04-01 23:01:43

Priority:

Medium     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

STAMP

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

08r1-8

App binary format:

N/A     

Summary: trunk kernel build joystick fails

Details:

 

trunk kernel build joystick fails.

 

rm -f linux-2.6.x/usr/initramfs_data.cpio.gz

make ARCH=blackfin   CROSS_COMPILE=bfin-uclinux- -j1 -C linux-2.6.x  || exit 1

make[1]: Entering directory `/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x'

  SYMLINK include/asm-blackfin/mach-bf537 -> include/asm-blackfin/mach

  CHK     include/linux/version.h

  CHK     include/linux/utsrelease.h

  CALL    scripts/checksyscalls.sh

  CHK     include/linux/compile.h

  GEN     usr/initramfs_data.cpio.gz

  AS      usr/initramfs_data.o

  LD      usr/built-in.o

  CC      arch/blackfin/mach-bf537/boards/stamp.o

  LD      arch/blackfin/mach-bf537/boards/built-in.o

  GZIP    kernel/config_data.gz

  IKCFG   kernel/config_data.h

  CC      kernel/configs.o

  LD      kernel/built-in.o

  CC      drivers/i2c/i2c-core.o

  CC      drivers/i2c/i2c-dev.o

  CC      drivers/i2c/busses/i2c-bfin-twi.o

  LD      drivers/i2c/busses/built-in.o

  LD      drivers/i2c/built-in.o

  CC      drivers/input/joydev.o

  CC      drivers/input/evdev.o

  LD      drivers/input/joystick/built-in.o

  CC [M]  drivers/input/joystick/ad7142.o

drivers/input/joystick/ad7142.c: In function 鈥榓d7142_probe鈥�

drivers/input/joystick/ad7142.c:437: error: implicit declaration of function 鈥楲ONG鈥

drivers/input/joystick/ad7142.c:437: warning: left shift count >= width of type

drivers/input/joystick/ad7142.c:437: warning: left shift count >= width of type

drivers/input/joystick/ad7142.c:438: warning: left shift count >= width of type

drivers/input/joystick/ad7142.c:438: warning: left shift count >= width of type

drivers/input/joystick/ad7142.c:439: warning: left shift count >= width of type

drivers/input/joystick/ad7142.c:439: warning: left shift count >= width of type

drivers/input/joystick/ad7142.c:440: warning: left shift count >= width of type

drivers/input/joystick/ad7142.c:440: warning: left shift count >= width of type

make[4]: *** [drivers/input/joystick/ad7142.o] Error 1

make[3]: *** [drivers/input/joystick] Error 2

make[2]: *** [drivers/input] Error 2

make[1]: *** [drivers] Error 2

make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x'

make: *** [linux] Error 1

ERROR: Error somewhere during make

 

Follow-ups

 

--- Sonic Zhang                                              2008-03-17 00:41:33

Graf,

 

Could you take a look?

 

--- Graf Yang                                                2008-03-17 04:17:19

The old macros LONG(), BIT() that are used in ad7142.c, in input.h have been

ommitted, so there are build errors. Now we use bit-ops macros defined in

linux/bitops.h.

 

--- Mingquan Pan                                             2008-04-01 23:01:42

Fixed.Close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes