[#3959] Unplug MMC card from SPI-MMC daughter card, system hangs and takes long time to recover.

Document created by Aaronwu Employee on Aug 28, 2013
Version 1Show Document
  • View in full screen mode

[#3959] Unplug MMC card from SPI-MMC daughter card, system hangs and takes long time to recover.

Submitted By: Vivi Li

Open Date

2008-03-06 03:12:08     Close Date

2008-03-14 06:33:46

Priority:

Medium High     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

08r1-8

App binary format:

N/A     

Summary: Unplug MMC card from SPI-MMC daughter card, system hangs and takes long time to recover.

Details:

 

Plug in a MMC card in SPI-MMC daughter card, the card can be detected.

Then unplug the MMC card, system will not respond for a long time. It may take half minute or longer to respond to key input in the console.

It's OK for SD card that I tested. This happens both in trunk and 08r1 branch.

 

Follow-ups

 

--- Graf Yang                                                2008-03-10 23:24:28

When unpluging the MMC card, the card detect handler will call

spi_mmc_revalidate() 'immediately', this cause the console not response. Now

have fixed.

 

--- Vivi Li                                                  2008-03-14 05:47:51

I validate with all SD/MMC cards and found it fails to detect all my SanDisk SD

cards when I plug them into SD slot after kernel boot up.

 

Plug it to SD slot before kernel boot up, it can be detected.

 

--- Vivi Li                                                  2008-03-14 06:33:46

SanDisk SD cards auto detection problem is not related to this bug. I will open

a new one.

This bug is fixed. Close it.

Thank you!

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes