[#3907] For AD1836, it fails to play wav audio with particular settings by alsa lib tool

Document created by Aaronwu Employee on Aug 28, 2013
Version 1Show Document
  • View in full screen mode

[#3907] For AD1836, it fails to play wav audio with particular settings by alsa lib tool

Submitted By: Vivi Li

Open Date

2008-02-18 05:14:12     Close Date

2008-03-04 23:15:46

Priority:

Medium     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

toochain 08r1-8

App binary format:

N/A     

Summary: For AD1836, it fails to play wav audio with particular settings by alsa lib tool

Details:

 

In 08r1 branch, for AD1836, use alsa lib tool to record a wav stereo audio with 8k sample rate and U8 format, then play it with aplay. It will fail.

This bug happens on both bf533-stamp and bf537-stamp.

 

Below is the log:

--

Linux version 2.6.22.18-ADI-2008R1-svn4263 (test@uclinux142-usb176x) (gcc version 4.1.2 (ADI svn)) #15 Fri Feb 15 11:00:24 GMT+8 2008

early printk enabled on early_BFuart0

Hardware Trace Active and Enabled

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Blackfin support (C) 2004-2007 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 100 MHz System Clock

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  text      = 0x00001000-0x001179b0

  rodata    = 0x00118000-0x0016632c

  data      = 0x00167000-0x0017a000

    stack   = 0x00168000-0x0016a000

  init      = 0x0017a000-0x00550000

  bss       = 0x00550000-0x0055faf0

  available = 0x0055faf0-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

Instruction Cache Enabled

Data Cache Enabled (write-through)

Built 1 zonelists.  Total pages: 14224

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:1:eth0:of

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 51260k/65536k RAM, (3928k init code, 1114k kernel code, 456k data, 1024k dma, 7756k reserved)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin Data A SRAM: 16 KB (15 KB free)

Blackfin Data B SRAM: 16 KB (16 KB free)

Blackfin Instruction SRAM: 48 KB (39 KB free)

Security Framework v1.0.0 initialized

Mount-cache hash table entries: 512

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

Generic PHY: Registered new driver

NET: Registered protocol family 2

                                  IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Dynamic Power Management Controller Driver v0.1: major=10, minor = 254

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

RAMDISK driver initialized: 16 RAM disks of 4096K size 1024 blocksize

SMSC LAN83C185: Registered new driver

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=19)@sclk=100MHz)

bfin_mac: Version 1.1, Blackfin BF53[67] BF527 on-chip Ethernet MAC driver

bfin-spi bfin-spi.0: Blackfin BF5xx on-chip SPI Contoller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).

dma_alloc_init: dma_page @ 0x03391000 - 256 pages at 0x03f00000

ALSA device list:

  #0: ADI ad1836 at PF4 SPORT0 rx/tx dma 3/4 err irq 45

TCP cubic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting the system clock to 1970-01-01 00:38:48 (2328)

IP-Config: Complete:

      device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=1, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 3928k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.4.1 (2008-02-15 10:55:34 GMT+8) Built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/> PHY: 0:01 - Link is Up - 100/Full

root:/>

root:/> arecord -t wav -c 2 -f U8 -r 8000 -d 5 wav

Recording WAVE 'wav' : Unsigned 8 bit, Rate 8000 Hz, Stereo

root:/> aplay wav

Playing WAVE 'wav' : Unsigned 8 bit, Rate 8000 Hz, Stereo

Data access misaligned address violation

- Attempted misaligned data memory or data cache access.

Defered Exception context

CURRENT PROCESS:

COMM=aplay PID=125

TEXT = 0x009c0000-0x009cb900  DATA = 0x00970900-0x00971504

BSS = 0x00971504-0x00980000   USER-STACK = 0x0099feb0

 

return address: [0x00258dce]; contents of:

0x00258da0:  2fce  3204  e579  fff2  c604  0009  4e40  4b38

0x00258db0:  9700  2fc5  e578  fff2  c682  8240  6008  4fb8

0x00258dc0:  5401  0c00  1c50  63f8  4fc0  5601  3214 [9310]

0x00258dd0:  2fb6  e578  fff2  4b78  c682  8240  48b9  1c3e

 

SEQUENCER STATUS:               Not tainted

SEQSTAT: 00060024  IPEND: 0030  SYSCFG: 0006

  HWERRCAUSE: 0x18

  EXCAUSE   : 0x24

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x004de000> [ aplay + 0x0 ]

RETX: <0x00258dce> [ /usr/lib/libasound.so.2 + 0x58dce ]

RETS: <0x00258ae0> [ /usr/lib/libasound.so.2 + 0x58ae0 ]

PC  : <0x00258dce> [ /usr/lib/libasound.so.2 + 0x58dce ]

DCPLB_FAULT_ADDR: <0x009302ac> [ aplay + 0x2ac ]

ICPLB_FAULT_ADDR: <0x00258dce> [ /usr/lib/libasound.so.2 + 0x58dce ]

 

PROCESSOR STATE:

R0 : 07000000    R1 : 00000000    R2 : 00000700    R3 : 00000000

R4 : 009302ae    R5 : 00000000    R6 : 009b63b8    R7 : 00000700

P0 : 00000020    P1 : 0092f0b0    P2 : 009302ae    P3 : 037abd80

P4 : 00918a6c    P5 : 00930004    FP : 0099f96c    SP : 004ddf24

LB0: 0092f0c5    LT0: 0092f0b8    LC0: 00000000

LB1: 00246d55    LT1: 00246d4e    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 00976006

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 00000000

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 0099f79c

A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000

USP : 0099f928  ASTAT: 02002020

 

Hardware Trace:

   0 Target : <0x000047e0> { _trap_c + 0x0 }

     Source : <0xffa0076c> { _exception_to_level5 + 0xb4 }

   1 Target : <0xffa006b8> { _exception_to_level5 + 0x0 }

     Source : <0xffa00614> { _ex_trap_c + 0x5c }

   2 Target : <0xffa005b8> { _ex_trap_c + 0x0 }

     Source : <0xffa0080c> { _trap + 0x28 }

   3 Target : <0xffa007e4> { _trap + 0x0 }

     Source : <0x00258dcc> [ /usr/lib/libasound.so.2 + 0x58dcc ]

   4 Target : <0x00258dcc> [ /usr/lib/libasound.so.2 + 0x58dcc ]

     Source : <0x00258df2> [ /usr/lib/libasound.so.2 + 0x58df2 ]

   5 Target : <0x00258dec> [ /usr/lib/libasound.so.2 + 0x58dec ]

     Source : <0x00258afa> [ /usr/lib/libasound.so.2 + 0x58afa ]

   6 Target : <0x00258ae0> [ /usr/lib/libasound.so.2 + 0x58ae0 ]

     Source : <0x0092f0cc> [ /lib/libm-0.9.29.so + 0xf0cc ]

   7 Target : <0x0092f0b0> [ /lib/libm-0.9.29.so + 0xf0b0 ]

     Source : <0x00228b34> [ /usr/lib/libasound.so.2 + 0x28b34 ]

   8 Target : <0x00228b2c> [ /usr/lib/libasound.so.2 + 0x28b2c ]

     Source : <0x00258adc> [ /usr/lib/libasound.so.2 + 0x58adc ]

   9 Target : <0x00258ac2> [ /usr/lib/libasound.so.2 + 0x58ac2 ]

     Source : <0x00258bb2> [ /usr/lib/libasound.so.2 + 0x58bb2 ]

  10 Target : <0x00258baa> [ /usr/lib/libasound.so.2 + 0x58baa ]

     Source : <0x00258aa6> [ /usr/lib/libasound.so.2 + 0x58aa6 ]

  11 Target : <0x002589c0> [ /usr/lib/libasound.so.2 + 0x589c0 ]

     Source : <0x0025849c> [ /usr/lib/libasound.so.2 + 0x5849c ]

  12 Target : <0x0025848c> [ /usr/lib/libasound.so.2 + 0x5848c ]

     Source : <0x002577fa> [ /usr/lib/libasound.so.2 + 0x577fa ]

  13 Target : <0x002577dc> [ /usr/lib/libasound.so.2 + 0x577dc ]

     Source : <0x0025774e> [ /usr/lib/libasound.so.2 + 0x5774e ]

  14 Target : <0x0025772c> [ /usr/lib/libasound.so.2 + 0x5772c ]

     Source : <0x0025788c> [ /usr/lib/libasound.so.2 + 0x5788c ]

  15 Target : <0x0025786a> [ /usr/lib/libasound.so.2 + 0x5786a ]

     Source : <0x00246ec6> [ /usr/lib/libasound.so.2 + 0x46ec6 ]

Stack from 004ddf04:

        009b63b8 ffa00770 0016c568 0016c568 0016c568 00000000 00000001 0084d068

        00258dce 00000030 00060024 00000000 004de000 00258dce 00258dce 00258ae0

        07000000 02002020 00246d55 0092f0c5 00246d4e 0092f0b8 00000000 00000000

        00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

        00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

        0099f79c 00000000 00000000 00976006 0099f928 0099f96c 00930004 00918a6c

 

Call Trace:

 

Bus error

root:/>

--

 

Follow-ups

 

--- Vivi Li                                                  2008-02-18 06:23:59

On bf537-stamp with ad1836, run test script two_channel_ad1836_audio_test.exp,

similar errors occur.

 

Below is the log:

--

root:/> arecord -t wav -c 2 -f U8 -r 44100 -d 5 wav1; arecord -t wav -c 2 -f

S16_LE -r 8000 -d 5 wav2

Recording WAVE 'wav1' : Unsigned 8 bit, Rate 44100 Hz, Stereo

Recording WAVE 'wav2' : Signed 16 bit Little Endian, Rate 8000 Hz, Stereo

root:/> aplay wav1&

165

root:/> Playing WAVE 'wav1' : Unsigned 8 bit, Rate 44100 Hz, Stereo

 

root:/> Data access misaligned address violation

- Attempted misaligned data memory or data cache access.

Defered Exception context

CURRENT PROCESS:

COMM=aplay PID=165

TEXT = 0x009e0000-0x009eb900  DATA = 0x002c6900-0x002c7504

BSS = 0x002c7504-0x00320000   USER-STACK = 0x0033feb0

 

return address: [0x00a58dce]; contents of:

0x00a58da0:  2fce  3204  e579  fff2  c604  0009  4e40  4b38 

0x00a58db0:  9700  2fc5  e578  fff2  c682  8240  6008  4fb8 

0x00a58dc0:  5401  0c00  1c50  63f8  4fc0  5601  3214 [9310]

0x00a58dd0:  2fb6  e578  fff2  4b78  c682  8240  48b9  1c3e 

 

SEQUENCER STATUS:        Not tainted

SEQSTAT: 00002024  IPEND: 0030  SYSCFG: 0006

  HWERRCAUSE: 0x0

  EXCAUSE   : 0x24

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x037d0000> /* unknown address */

RETX: <0x00a58dce> [ /usr/lib/libasound.so.2 + 0x58dce ]

RETS: <0x00a58ae0> [ /usr/lib/libasound.so.2 + 0x58ae0 ]

PC  : <0x00a58dce> [ /usr/lib/libasound.so.2 + 0x58dce ]

DCPLB_FAULT_ADDR: <0x002c8eb4> [ aplay + 0xeb4 ]

ICPLB_FAULT_ADDR: <0x00a58dce> [ /usr/lib/libasound.so.2 + 0x58dce ]

 

PROCESSOR STATE:

R0 : fb000000    R1 : 00000000    R2 : 0000fb00    R3 : 00000000

R4 : 002c8eb6    R5 : 00000000    R6 : 009663b8    R7 : 0000fc00

P0 : 00000020    P1 : 004df0b0    P2 : 002c8eb6    P3 : 009a5d80

P4 : 00214790    P5 : 002c8004    FP : 0033f96c    SP : 037cff24

LB0: 004df0c5    LT0: 004df0b8    LC0: 00000000

LB1: 00a46d55    LT1: 00a46d4e    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 002a4eb8

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 00000000

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 0033f79c

A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000

USP : 0033f928  ASTAT: 02002022

 

Hardware Trace:

   0 Target : <0x000047e0> { _trap_c + 0x0 }

     Source : <0xffa0076c> { _exception_to_level5 + 0xb4 }

   1 Target : <0xffa006b8> { _exception_to_level5 + 0x0 }

     Source : <0xffa00614> { _ex_trap_c + 0x5c }

   2 Target : <0xffa005b8> { _ex_trap_c + 0x0 }

     Source : <0xffa0080c> { _trap + 0x28 }

   3 Target : <0xffa007e4> { _trap + 0x0 }

     Source : <0x00a58dcc> [ /usr/lib/libasound.so.2 + 0x58dcc ]

   4 Target : <0x00a58dcc> [ /usr/lib/libasound.so.2 + 0x58dcc ]

     Source : <0x00a58df2> [ /usr/lib/libasound.so.2 + 0x58df2 ]

   5 Target : <0x00a58dec> [ /usr/lib/libasound.so.2 + 0x58dec ]

     Source : <0x00a58afa> [ /usr/lib/libasound.so.2 + 0x58afa ]

   6 Target : <0x00a58ae0> [ /usr/lib/libasound.so.2 + 0x58ae0 ]

     Source : <0x004df0cc> [ /lib/libm-0.9.29.so + 0xf0cc ]

   7 Target : <0x004df0b0> [ /lib/libm-0.9.29.so + 0xf0b0 ]

     Source : <0x00a28b34> [ /usr/lib/libasound.so.2 + 0x28b34 ]

   8 Target : <0x00a28b2c> [ /usr/lib/libasound.so.2 + 0x28b2c ]

     Source : <0x00a58adc> [ /usr/lib/libasound.so.2 + 0x58adc ]

   9 Target : <0x00a58ac2> [ /usr/lib/libasound.so.2 + 0x58ac2 ]

     Source : <0x00a58bb2> [ /usr/lib/libasound.so.2 + 0x58bb2 ]

  10 Target : <0x00a58baa> [ /usr/lib/libasound.so.2 + 0x58baa ]

     Source : <0x00a58aa6> [ /usr/lib/libasound.so.2 + 0x58aa6 ]

  11 Target : <0x00a589c0> [ /usr/lib/libasound.so.2 + 0x589c0 ]

     Source : <0x00a5849c> [ /usr/lib/libasound.so.2 + 0x5849c ]

  12 Target : <0x00a5848c> [ /usr/lib/libasound.so.2 + 0x5848c ]

     Source : <0x00a577fa> [ /usr/lib/libasound.so.2 + 0x577fa ]

  13 Target : <0x00a577dc> [ /usr/lib/libasound.so.2 + 0x577dc ]

     Source : <0x00a5774e> [ /usr/lib/libasound.so.2 + 0x5774e ]

  14 Target : <0x00a5772c> [ /usr/lib/libasound.so.2 + 0x5772c ]

     Source : <0x00a5788c> [ /usr/lib/libasound.so.2 + 0x5788c ]

  15 Target : <0x00a5786a> [ /usr/lib/libasound.so.2 + 0x5786a ]

     Source : <0x00a46ec6> [ /usr/lib/libasound.so.2 + 0x46ec6 ]

Stack from 037cff04:

        009663b8 ffa00770 0016c56c 0016c56c 0016c568 00000000 00000002 0084d068

 

        00a58dce 00000030 00002024 00000000 037d0000 00a58dce 00a58dce 00a58ae0

 

        fb000000 02002022 00a46d55 004df0c5 00a46d4e 004df0b8 00000000 00000000

 

        00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

 

        00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

 

        0033f79c 00000000 00000000 002a4eb8 0033f928 0033f96c 002c8004 00214790

 

 

Call Trace:

[<0000fc00>] _do_exit+0x190/0x760

[<0000fb00>] _do_exit+0x90/0x760

 

aplay wav2

165: Bus error

Playing WAVE 'wav2' : Signed 16 bit Little Endian, Rate 8000 Hz, Stereo

root:/>

Case 13 ...PASS

 

Case 13 ...PASS

arecord -t wav -c 2 -f S16_LE -r 44100 -d 5 wav1; arecord -t wav -c 2 -f   U8

-r 8000 -d 5 wav2

Recording WAVE 'wav1' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo

Recording WAVE 'wav2' : Unsigned 8 bit, Rate 8000 Hz, Stereo

root:/> aplay wav1&

169

root:/> Playing WAVE 'wav1' : Signed 16 bit Little Endian, Rate 44100 Hz,

Stereo

 

root:/> aplay wav2

Playing WAVE 'wav2' : Unsigned 8 bit, Rate 8000 Hz, Stereo

Data access misaligned address violation

- Attempted misaligned data memory or data cache access.

Defered Exception context

CURRENT PROCESS:

COMM=aplay PID=170

TEXT = 0x009e0000-0x009eb900  DATA = 0x00318900-0x00319504

BSS = 0x00319504-0x00360000   USER-STACK = 0x0037feb0

 

return address: [0x00a58dce]; contents of:

0x00a58da0:  2fce  3204  e579  fff2  c604  0009  4e40  4b38 

0x00a58db0:  9700  2fc5  e578  fff2  c682  8240  6008  4fb8 

0x00a58dc0:  5401  0c00  1c50  63f8  4fc0  5601  3214 [9310]

0x00a58dd0:  2fb6  e578  fff2  4b78  c682  8240  48b9  1c3e 

 

SEQUENCER STATUS:        Not tainted

SEQSTAT: 00062024  IPEND: 0030  SYSCFG: 0006

  HWERRCAUSE: 0x18

  EXCAUSE   : 0x24

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x002b8000> [ aplay + 0x0 ]

RETX: <0x00a58dce> [ /usr/lib/libasound.so.2 + 0x58dce ]

RETS: <0x00a58ae0> [ /usr/lib/libasound.so.2 + 0x58ae0 ]

PC  : <0x00a58dce> [ /usr/lib/libasound.so.2 + 0x58dce ]

DCPLB_FAULT_ADDR: <0x009d02ac> [ aplay + 0x2ac ]

ICPLB_FAULT_ADDR: <0x00a58dce> [ /usr/lib/libasound.so.2 + 0x58dce ]

 

PROCESSOR STATE:

R0 : 0a000000    R1 : 00000000    R2 : 00000a00    R3 : 00000000

R4 : 009d02ae    R5 : 00000000    R6 : 009963b8    R7 : 00000500

P0 : 00000020    P1 : 004df0b0    P2 : 009d02ae    P3 : 00231d80

P4 : 002338c8    P5 : 009d0004    FP : 0037f96c    SP : 002b7f24

LB0: 004df0c5    LT0: 004df0b8    LC0: 00000000

LB1: 00a46d55    LT1: 00a46d4e    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 0023e006

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 00000000

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 0037f79c

A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000

USP : 0037f928  ASTAT: 02002020

 

Hardware Trace:

   0 Target : <0x000047e0> { _trap_c + 0x0 }

     Source : <0xffa0076c> { _exception_to_level5 + 0xb4 }

   1 Target : <0xffa006b8> { _exception_to_level5 + 0x0 }

     Source : <0xffa00614> { _ex_trap_c + 0x5c }

   2 Target : <0xffa005b8> { _ex_trap_c + 0x0 }

     Source : <0xffa0080c> { _trap + 0x28 }

   3 Target : <0xffa007e4> { _trap + 0x0 }

     Source : <0x00a58dcc> [ /usr/lib/libasound.so.2 + 0x58dcc ]

   4 Target : <0x00a58dcc> [ /usr/lib/libasound.so.2 + 0x58dcc ]

     Source : <0x00a58df2> [ /usr/lib/libasound.so.2 + 0x58df2 ]

   5 Target : <0x00a58dec> [ /usr/lib/libasound.so.2 + 0x58dec ]

     Source : <0x00a58afa> [ /usr/lib/libasound.so.2 + 0x58afa ]

   6 Target : <0x00a58ae0> [ /usr/lib/libasound.so.2 + 0x58ae0 ]

     Source : <0x004df0cc> [ /lib/libm-0.9.29.so + 0xf0cc ]

   7 Target : <0x004df0b0> [ /lib/libm-0.9.29.so + 0xf0b0 ]

     Source : <0x00a28b34> [ /usr/lib/libasound.so.2 + 0x28b34 ]

   8 Target : <0x00a28b2c> [ /usr/lib/libasound.so.2 + 0x28b2c ]

     Source : <0x00a58adc> [ /usr/lib/libasound.so.2 + 0x58adc ]

   9 Target : <0x00a58ac2> [ /usr/lib/libasound.so.2 + 0x58ac2 ]

     Source : <0x00a58bb2> [ /usr/lib/libasound.so.2 + 0x58bb2 ]

  10 Target : <0x00a58baa> [ /usr/lib/libasound.so.2 + 0x58baa ]

     Source : <0x00a58aa6> [ /usr/lib/libasound.so.2 + 0x58aa6 ]

  11 Target : <0x00a589c0> [ /usr/lib/libasound.so.2 + 0x589c0 ]

     Source : <0x00a5849c> [ /usr/lib/libasound.so.2 + 0x5849c ]

  12 Target : <0x00a5848c> [ /usr/lib/libasound.so.2 + 0x5848c ]

     Source : <0x00a577fa> [ /usr/lib/libasound.so.2 + 0x577fa ]

  13 Target : <0x00a577dc> [ /usr/lib/libasound.so.2 + 0x577dc ]

     Source : <0x00a5774e> [ /usr/lib/libasound.so.2 + 0x5774e ]

  14 Target : <0x00a5772c> [ /usr/lib/libasound.so.2 + 0x5772c ]

     Source : <0x00a5788c> [ /usr/lib/libasound.so.2 + 0x5788c ]

  15 Target : <0x00a5786a> [ /usr/lib/libasound.so.2 + 0x5786a ]

     Source : <0x00a46ec6> [ /usr/lib/libasound.so.2 + 0x46ec6 ]

Stack from 002b7f04:

        009963b8 ffa00770 0016c570 0016c570 0016c568 00000000 00000001 0084d068

 

        00a58dce 00000030 00062024 00000000 002b8000 00a58dce 00a58dce 00a58ae0

 

        0a000000 02002020 00a46d55 004df0c5 00a46d4e 004df0b8 00000000 00000000

 

        00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

 

        00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

 

        0037f79c 00000000 00000000 0023e006 0037f928 0037f96c 009d0004 002338c8

 

 

Call Trace:

 

Bus error

root:/>

--

 

--- Cliff Cai                                                2008-02-19 22:31:24

set period number to 8 at least to avoid accessing misaligned address in 32bit

mode

 

--- Vivi Li                                                  2008-03-04 23:15:44

It's ok now for both BF533-STAMP and BF537-STAMP. Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes