[#3905] Can't found eth0 device on EZKIT-548 with svn trunk kernel

Document created by Aaronwu Employee on Aug 28, 2013
Version 1Show Document
  • View in full screen mode

[#3905] Can't found eth0 device on EZKIT-548 with svn trunk kernel

Submitted By: Bryan Wu

Open Date

2008-02-18 03:49:40     Close Date

2008-02-21 01:55:15

Priority:

Medium     Assignee:

Bryan Wu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

EZKIT Lite

Processor:

BF548     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

App binary format:

N/A     

Summary: Can't found eth0 device on EZKIT-548 with svn trunk kernel

Details:

 

--

Linux version 2.6.24.2-ADI-2008R2-pre-svn4288 (roc@roc-desktop) (gcc version 4.1.2 (ADI svn)) #29 Mon Feb 18 16:34:02 CST 2008

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001921b0

  rodata    = 0x001922e0-0x00213b3c

  bss       = 0x00213b40-0x00227224

  data      = 0x00227224-0x00244000

    stack   = 0x00242000-0x00244000

  init      = 0x00244000-0x006ba000

  available = 0x006ba000-0x03dff000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace Active and Enabled

Blackfin support (C) 2004-2008 Analog Devices, Inc.

Compiled for ADSP-BF548 Rev 0.0

Warning: Compiled for Rev 0, but running on Rev 1

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

Instruction Cache Enabled

Data Cache Enabled (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 15748

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart1,57600 console=ttyBF0,57600 ip=192.168.0.66:192.168.0.55:192.168.0.1:2f

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

Console: colour dummy device 80x25

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 56012k/65536k RAM, (4568k init code, 1604k kernel code, 712k data, 2048k dma, 588k reserved)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin Data A SRAM: 16 KB (15 KB free)

Blackfin Data B SRAM: 16 KB (16 KB free)

Blackfin Instruction SRAM: 48 KB (42 KB free)

Security Framework initialized

Mount-cache hash table entries: 512

net_namespace: 64 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

ezkit_init(): registering device resources

SCSI subsystem initialized

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bf54x-lq043: FrameBuffer initializing...

dma_alloc_init: dma_page @ 0x0342b000 - 512 pages at 0x03e00000

Console: switching to colour frame buffer device 80x24

bfin-otp: initialized

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc02000 (irq = 48) is a BFIN-UART

RAMDISK driver initialized: 16 RAM disks of 4096K size 1024 blocksize

smsc911x: Driver version 2007-07-13.

Driver 'sd' needs updating - please use bus_type methods

Driver 'sr' needs updating - please use bus_type methods

register bfin atapi driver

scsi0 : pata-bf54x

ata1: PATA max UDMA/66 irq 68

ata1.00: ATA-6: TOSHIBA MK4032GAX, AD101A, max UDMA/100

ata1.00: 78140160 sectors, multi 16: LBA48

ata1.00: configured for UDMA/66

blk_queue_max_hw_segments: set to minimum 1

scsi 0:0:0:0: Direct-Access     ATA      TOSHIBA MK4032GA AD10 PQ: 0 ANSI: 5

sd 0:0:0:0: [sda] 78140160 512-byte hardware sectors (40008 MB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

sd 0:0:0:0: [sda] 78140160 512-byte hardware sectors (40008 MB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

sda: sda1

sd 0:0:0:0: [sda] Attached SCSI disk

physmap platform flash device: 01000000 at 20000000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank

Intel/Sharp Extended Query Table at 0x010A

  Unknown Intel/Sharp Extended Query version 1.5.

gen_probe: No supported Vendor Command Set found

physmap-flash physmap-flash.0: map_probe failed

BF5xx on-chip NAND FLash Controller Driver, Version 1.2 (c) 2007 Analog Devices, Inc.

bf5xx-nand bf5xx-nand.0: page_size=256, data_width=8, wr_dly=3, rd_dly=3

NAND device: Manufacturer ID: 0x20, Chip ID: 0xda (ST Micro NAND 256MiB 3,3V 8-bit)

Creating 2 MTD partitions on "NAND 256MiB 3,3V 8-bit":

0x00000000-0x00400000 : "Linux Kernel"

0x00400000-0x10000000 : "File System"

bfin-spi bfin-spi.0: Blackfin BF5xx on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@4

bfin-spi bfin-spi.1: Blackfin BF5xx on-chip SPI Controller Driver, Version 1.0, regs_base@ffc02300, dma channel@5

input: bf54x-keys as /class/input/input0

bf54x-keys: Blackfin BF54x Keypad registered IRQ 76

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

i2c /dev entries driver

i2c-bfin-twi i2c-bfin-twi.1: Blackfin BF5xx on-chip I2C TWI Contoller Driver, Version 1.8, regs_base@ffc02200

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).

ASoC version 0.13.1

AD1980 SoC Audio Codec

asoc: AC97 <-> bf5xx-ac97 mapping ok

ALSA device list:

  #0: bf5xx-board (AD1980-MMAP)

TCP cubic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 07:25:47 UTC (26747)

IP-Config: Failed to open eth0

IP-Config: Device `eth0' not found.

Freeing unused kernel memory: 4568k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.9.1 (2008-02-18 12:18:40 CST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/> ifconfig

lo        Link encap:Local Loopback 

          inet addr:127.0.0.1  Mask:255.0.0.0

          UP LOOPBACK RUNNING  MTU:16436  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

         

root:/> ifconfig eth0 up

SIOCSIFFLAGS: Invalid argument

root:/>

---

 

Follow-ups

 

--- Bryan Wu                                                 2008-02-18 04:43:31

it is fixed in svn kernel trunk.

 

-Bryan

 

--- Bryan Wu                                                 2008-02-21 01:55:14

close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes