[#3875] UART2, UART3 fail to build

Document created by Aaronwu Employee on Aug 28, 2013
Version 1Show Document
  • View in full screen mode

[#3875] UART2, UART3 fail to build

Submitted By: Rob D

Open Date

2008-01-31 11:01:56     Close Date

2008-04-01 17:01:16

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

2008r1-rc1

Category:

Drivers     Board:

EZKIT Lite

Processor:

BF548     Silicon Revision:

0.1

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

1.1.6-svn1118     Toolchain version or rev.:

svn r2153

App binary format:

N/A     

Summary: UART2, UART3 fail to build

Details:

 

Hi Guys..

 

When I enable UART2 and/or UART3 in the kernel config, the kernel fails to build.

 

bfin_serial_5xx.h

 

IRQ_UART2_RX

CH_UART2_TX

CH_UART2_RX

IRQ_UART3_RX

CH_UART3_TX

CH_UART3_RX

 

are undefined...  The board is in a lab and is somewhat painful to get a copy/paste of the build log... but if you need it, I'll get it.

 

Thanks!

 

-Rob

 

Follow-ups

 

--- Sonic Zhang                                              2008-02-02 03:03:50

Add UART2/UART3 DMA channel numbers and IRQ numbers.

Set proper DMA PMAP in request_dma().

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes