[#3837] rtc ioctl RTC_IRQP_SET error

Document created by Aaronwu Employee on Aug 28, 2013
Version 1Show Document
  • View in full screen mode

[#3837] rtc ioctl RTC_IRQP_SET error

Submitted By: Mingquan Pan

Open Date

2008-01-17 00:54:27     Close Date

2008-01-17 20:01:25

Priority:

Medium     Assignee:

Mike Frysinger

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

Oct 07

App binary format:

N/A     

Summary: rtc ioctl RTC_IRQP_SET error

Details:

 

rtc ioctl RTC_IRQP_SET error for Unknown error 515.

 

cd /bin^M

root:/bin> ./rtc_test^M

====== RTC Test  ====^M

0. open and release^M

opened '/dev/rtc0': fd = 3^M

1. ioctl RTC_UIE_ON^M

2. RTC read 5 times^M

PHY: 0:01 - Link is Up - 100/Full^M

RTC read 1^M

RTC read 2^M

RTC read 3^M

RTC read 4^M

RTC read 5^M

3. ioctl RTC_UIE_OFF^M

4. Get RTC Time^M

Current RTC date/time is 1-1-70, 11:48:22^M

5. Set RTC Time^M

Set Current RTC date/time to 31-5-104, 02:30:00^M

Get RTC time^M

Current RTC date/time is 31-5-104, 02:30:01^M

6. Set alarm Time^M

7. Get alarm Time^M

Alarm time now set to 02:30:51^M

Waiting 50 seconds for alarm...^M

Okay. Alarm rang.^M

Current RTC date/time is 31-5-104, 02:30:51^M

8. ioctl RTC_AIE_OFF^M

8.5 test sleep 10^M

Current RTC date/time is 31-5-104, 02:31:01^M

9. ioctl RTC_PIE_ON^M

Current RTC date/time is 31-5-104, 02:31:02^M

10. ioctl RTC_IRQP_SET^M

ioctl RTC_IRQP_SET error: Unknown error 515^M

Current RTC date/time is 31-5-104, 02:31:04^M

11. ioctl RTC_PIE_OFF^M

Current RTC date/time is 31-5-104, 02:31:05^M

RTC Tests done !!^M

 

Follow-ups

 

--- Mike Frysinger                                           2008-01-17 03:37:34

this is expected behavior as the Blackfin RTC does not support changing of its

frequency, so trying to use IRQP_SET will fail

 

--- Mingquan Pan                                             2008-01-17 04:50:26

How this case didn't fail before if this feature is not supported?

 

--- Mike Frysinger                                           2008-01-17 04:59:20

it was incorrectly implemented before and the feature was claimed to be

supported when in reality it was not

 

--- Mike Frysinger                                           2008-01-17 05:19:54

to be clear, it is the Blackfin RTC hardware itself which is not able to support

changing of frequencies as defined by the Linux api.  the RTC hardware can go

from a frequency of 1HZ to 1/2^32HZ when the Linux api needs it to scale in the

other direction: 1HZ to 2^32HZ.

 

--- Mingquan Pan                                             2008-01-17 22:02:48

All right.Close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes