[#3829] strace is missing some syscalls

Document created by Aaronwu Employee on Aug 28, 2013
Version 1Show Document
  • View in full screen mode

[#3829] strace is missing some syscalls

Submitted By: Mike Frysinger

Open Date

2008-01-14 06:21:38     Close Date

2008-01-14 08:29:41

Priority:

Medium     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

App binary format:

N/A     

Summary: strace is missing some syscalls

Details:

 

an strace from linphone:

SYS_318(0x7, 0xef2564, 0x2bfaec, 0x2, 0xebb1be) = 0

SYS_329(0x2, 0x2, 0, 0xcd90b03, 0x2bf9e8) = 10

SYS_327(0xa, 0x1, 0x6, 0x2bf924, 0x4)   = 0

 

Follow-ups

 

--- Robin Getz                                               2008-01-14 08:49:26

We discussed at one time, making strace in maintainer mode all the time, so it

would grab the syscalls from the kernel when you built it.

 

I could not figure it out, but Is that doable?

 

-Robin

 

--- Mike Frysinger                                           2008-01-14 09:13:18

with Roy gone, we're going to have to get famil with the build system ... i'll

take a stab at it

 

--- Mike Frysinger                                           2008-01-14 10:30:07

it's not possible to generate the system call list automatically (for any

architecture) ... ive fixed the Blackfin list to match properly

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes