2009-09-09 07:54:01     uvcvideo: Failed to submit URB 0

Document created by Aaronwu Employee on Aug 27, 2013
Version 1Show Document
  • View in full screen mode

2009-09-09 07:54:01     uvcvideo: Failed to submit URB 0

xm ye (CHINA)

Message: 79706   

 

hi,

i am testing UVC WebCam with bf533-ezkit, my USB hos is ISP1362, the kernel is 2.6 28(have V4l2 UVC driver),and  with some forum friends's help now can  open device,but i come to another problem. the code snippets is here:

 

static int video_enable(struct vdIn *vd)

{

    int type = V4L2_BUF_TYPE_VIDEO_CAPTURE;

    int ret;

 

    ret = ioctl(vd->fd, VIDIOC_STREAMON, &type);

 

    if (ret < 0) {

    perror("Unable to start capture");

    return ret;

    }

    vd->isstreaming = 1;

    return 0;

}

 

 

the error message in the console is :

uvcvideo: Failed to submit URB 0 (-28).

Unable to start capture: No space left on device

 

 

 

the ioctl above control to start video capture ,it is the  part of  driver,so i don't know what  will the problem. Is the USB HCD driver problem?  it seem can detect my device well and can read PID,VID.

 

Also my WebCam can work 30 fps(frame per sec),but in my code used ioctl to configure the fps,it unsuccess.

 

Dose someone have  done same work can give some help?

QuoteReplyEditDelete

 

 

2009-09-10 02:12:28     Re: uvcvideo: Failed to submit URB 0

xm ye (CHINA)

Message: 79723   

 

i have find the problem :the ISP1362 don't support  ISO transfer.so i need to rewrite the isp1362-hcd.c. Someone have realize it or i must need refer to material to code it?

QuoteReplyEditDelete

 

 

2009-09-10 03:48:21     Re: uvcvideo: Failed to submit URB 0

Mike Frysinger (UNITED STATES)

Message: 79743   

 

we dont maintain any USB host controller driver, so really you should ask the vendor, or perhaps the general usb mailing list

QuoteReplyEditDelete

 

 

2011-09-05 08:06:46     Re: uvcvideo: Failed to submit URB 0

zanget zanget (FALKLAND ISLANDS (MALVINAS))

Message: 103281   

 

hi,xm ye.

 

have you made it works so far ?

 

i'd like to see if anyupdates here

Attachments

    Outcomes