2011-08-30 01:42:11     ad73322 +2010 + aplay + arecord

Document created by Aaronwu Employee on Aug 27, 2013
Version 1Show Document
  • View in full screen mode

2011-08-30 01:42:11     ad73322 +2010 + aplay + arecord

Shyam sundar (INDIA)

Message: 103182   

 

Hello world,

 

I am using ad73322 codec on a customised BF531 board with uclinux 2010 distribution.

 

The sampling rate used is 8KHz. When I give the following command to record the file being

 

played, sometimes I dont see any recorded samples,sometimes a part of the file being recorded

 

And sometimes I do see overruns and underruns

 

What could be the problem? I am using only a single chip

 

I am attaching the driver file !

 

arecord -f S16_LE -t wav -d 20 -r 8000 -c 1 test.wav &; aplay -f S16_LE

-t wav -r 8000 -c 1 /tones/tone800.wav

 

ad73322.c

Attachments

Outcomes