2011-08-29 01:30:35     Use CONFIG_RTC_HCTOSYS with rtc driver as module?

Document created by Aaronwu Employee on Aug 27, 2013
Version 1Show Document
  • View in full screen mode

2011-08-29 01:30:35     Use CONFIG_RTC_HCTOSYS with rtc driver as module?

Lukas Weiss (GERMANY)

Message: 103174   

 

Hello,

 

is it possible to use the HCTOSYS option to load the system time from RTC on bootup when the RTC driver is built as module? How do i load the module on boottime to make that work?

 

Thank you for some help

- Lukas

TranslateQuoteReplyEditDelete

 

 

2011-08-29 01:52:01     Re: Use CONFIG_RTC_HCTOSYS with rtc driver as module?

Aaron Wu (CHINA)

Message: 103176   

 

If you want the RTC driver immediately available at boot up, why not compile it into the kernel? Anyway you can do what you want with your scripts in /etc/init.d/rc, it get executed on boot up.

QuoteReplyEditDelete

Attachments

    Outcomes