2011-08-10 04:07:55     How i can create flash folder to load the application in flash memory

Document created by Aaronwu Employee on Aug 27, 2013
Version 1Show Document
  • View in full screen mode

2011-08-10 04:07:55     How i can create flash folder to load the application in flash memory

barreh walid (TUNISIA)

Message: 102881   

 

I have a BF548 ezkit and I am using the latest trunk kernel/uboot/filesystem ( 2010R1 ).

 

How i can create flash folder in flash memory to load the application after kernel boot up ?

 

 

QuoteReplyEditDelete

 

 

2011-08-10 05:22:04     Re: How i can create flash folder to load the application in flash memory

Aaron Wu (CHINA)

Message: 102882   

 

Creat a Flash file system on your flash, and mount your FLASH MTD device after boot up. please refer to   docs.blackfin.uclinux.org/doku.php?id=linux-kernel:jffs&s[]=jffs2 and   docs.blackfin.uclinux.org/doku.php?id=linux-kernel:mtd&s[]=mtd

Attachments

    Outcomes