2011-08-02 09:16:45     make xconfig fails on fedora 14

Document created by Aaronwu Employee on Aug 27, 2013
Version 1Show Document
  • View in full screen mode

2011-08-02 09:16:45     make xconfig fails on fedora 14

Chandrashekhar Lavania (INDIA)

Message: 102785   

 

Hi,

 

 

 

We are running Fedora 14 (2.6.35.13-92.fc14.i686 #1 SMP Sat May 21 17:39:42 UTC 2011 i686 i686 i386 GNU/Linux) and have installed the following packages.

 

 

 

Installed Packages:

 

autoconf automake bash binutils bison bzip2 coreutils flex gawk gcc

 

gettext grep intltool iputils libtool glibc-devel lzo lzo-devel

 

ncurses-libs m4 pax-utils pkgconfig rpm texinfo zlib

 

gpm gmp-devel mpfr mpfr-devel

 

gcc-c++ qt3-devel gtk2-devel libglade2-devel

 

ckermit diffstat ftp lrzsz mailx minicom rsh subversion tftp tree vim xinetd patch

 

libusb-devel libftdi-devel

 

install ncurses-devel

 

ncurses-devel

 

binutils install gcc glibc-devel ncurses zlib texinfo glibc-devel glibc-static lzo lzo-devel coreutils

 

ncurses ncurses-devel glibc-headers glibc-devel cpp binutils gcc tcl gtk2-devel qt-devel glib2-devel libglade2-devel

 

xorg-x11-server-devel

 

 

 

 

 

We tried "make clean" and "make" commands on the distro and was successfull. But "make xconfig" fails with the below mentioned error.

 

 

 

Command:

 

make xconfig

 

Error:

 

find vendors -mindepth 2 '(' -name .svn -prune ')' -o -type f -name Kconfig -print | sed 's:^:source ../:' > vendors/Kconfig

 

config/mkconfig > Kconfig

 

CC=cc CXX=c++ make -C /home/karthikeyan/TLL/Distro/uClinux-dist/config/kconfig gconf

 

make[1]: Entering directory `/home/karthikeyan/TLL/Distro/uClinux-dist/config/kconfig'

 

cc   gconf.o kconfig_load.o zconf.tab.o  -lncursesw `pkg-config --libs gtk+-2.0 gmodule-2.0 libglade-2.0` -o gconf

 

/usr/bin/ld: kconfig_load.o: undefined reference to symbol 'dlopen@@GLIBC_2.1'

 

/usr/bin/ld: note: 'dlopen@@GLIBC_2.1' is defined in DSO /lib/libdl.so.2 so try adding it to the linker command line

 

/lib/libdl.so.2: could not read symbols: Invalid operation

 

collect2: ld returned 1 exit status

 

make[1]: *** [gconf] Error 1

 

make[1]: Leaving directory `/home/karthikeyan/TLL/Distro/uClinux-dist/config/kconfig'

 

make: *** [/home/karthikeyan/TLL/Distro/uClinux-dist/config/kconfig/gconf] Error 2

 

 

 

What may be causing this issue?

 

 

 

Regards,

 

Shekhar

 

PS : In blackfin-ubuntu 0.9 and  ubuntu 9.10 we were able to do this properly.

 

PPS: make menuconfig works fine

QuoteReplyEditDelete

 

 

2011-08-03 00:10:17     Re: make xconfig fails on fedora 14

Chandrashekhar Lavania (INDIA)

Message: 102790   

 

Hi,

 

This isue may be resolved by doing the following on the terminal in the uClinux-dist directory when we make xconfig:

 

LDLIBS=-ldl make xconfig

 

 

 

Regards,

 

Shekhar

Attachments

    Outcomes