2011-07-11 15:21:17     Bus Error

Document created by Aaronwu Employee on Aug 27, 2013
Version 1Show Document
  • View in full screen mode

2011-07-11 15:21:17     Bus Error

Louis Ruch (SOUTH AFRICA)

Message: 102326   

 

Hey All,

 

I haven't had much time to run some proper tests, but I will do some more tommorrow.  I am based out of South Africa so just trying to get a head start on some assistance in case any of you can lead me in the correct direciton.

 

We have just finished building our custom made board using the BF537 processor.  I need to get a couple of C application running on this board.  I previously used a IP04 board and was able to get my apps running.

 

I have setup Eclipse Helios on my pc installed the 2008R1 RC8 toolchain for windows and using MinGW to get the make going.  The reason I am using the 2008R1 RC8 toolchain is because we built a the uImage using Astfin which still uses the 2008 toolchain.

 

I tried getting my TCP server running but all that happens is when I type ./TCPServer is it gives "Bus error".  After this I tried to get just a simple Hello World going and it gives the same error:

 

"Bus error"

 

From Ecilpse I just create new C project -> Hello World ANSI C -> Blackfin Linux FDPIC toolchain -> Finish

 

After this I build and gives this error.  Not sure where to start debugging because all I am doing is a printf??

 

Thanks!

QuoteReplyEditDelete

 

 

2011-07-11 15:44:38     Re: Bus Error

Mike Frysinger (UNITED STATES)

Message: 102327   

 

look at `dmesg` and see if there's anything useful logged

 

how are you transferring it to the board ?  if ftp, make sure you're using binary mode.

QuoteReplyEditDelete

 

 

2011-07-11 16:19:24     Re: Bus Error

Louis Ruch (SOUTH AFRICA)

Message: 102328   

 

Ah yes I have had trouble using Filezilla in the past will make sure its set to binary mode tommorrow quickly.

 

 

 

Louis

QuoteReplyEditDelete

 

 

2011-07-12 02:21:03     Re: Bus Error

Louis Ruch (SOUTH AFRICA)

Message: 102333   

 

Thanks Mike,

 

It was the medium I was using to get the file accross working now.

Attachments

    Outcomes