2011-06-22 03:23:35     nit: /sbin/syslogd respawning too fast - MSG in 2010R

Document created by Aaronwu Employee on Aug 27, 2013
Version 1Show Document
  • View in full screen mode

2011-06-22 03:23:35     nit: /sbin/syslogd respawning too fast - MSG in 2010R

Ganesh krish (INDIA)

Message: 101560   

 

Hi,

 

    I do get this message "init: /sbin/syslogd respawning too fast" everytime after boot  continuously .  Can U please help me with this ??

 

I made some changes in  "Customize Application/Library Settings"  . I'm not sure bcause of tht i'm getting this msg !!! Please clarify this ??

 

 

 

U-Boot 2010.06-svn2634 (ADI-2010R1) (Jun 20 2011 - 11:48:57)                                                             

                                                                                                                         

CPU:   ADSP bf531-0.3 (Detected Rev: 0.3) (spi flash boot)                                                               

Board: RITCoE BF531 DWAS board                                                                                           

       Support: ssmr@tcoe.iitm.ac.in                                                                                     

Clock: VCO: 294.912 MHz, Core: 294.912 MHz, System: 98.304 MHz                                                           

RAM:   32 MiB                                                                                                            

Flash: ## Unknown FLASH on Bank 1 - Size = 0x00000000 = 0 MB                                                             

0 Bytes                                                                                                                  

SF: Detected W25Q128 with page size 256 and flash size 16MB                                                              

In:    serial                                                                                                            

Out:   serial                                                                                                            

Err:   serial                                                                                                            

KGDB:  [on serial] ready                                                                                                 

Hit any key to stop autoboot:  0                                                                                         

bfin> loady

## Ready for binary (ymodem) download to 0x01000000 at 115200 bps...                                                     

C0(CAN) packets, 3 retries

## Total Size      = 0x002c0f0f = 2887439 Bytes

bfin> bootm

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   bf533-2.6.34.7-ADI-2010R1-svn958

   Created:      2011-06-22   6:53:34 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    2887375 Bytes = 2.8 MiB

   Load Address: 00001000

   Entry Point:  0010bb78

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 0010bb78

Linux version 2.6.34.7-ADI-2010R1-svn9581 (ganeshn@ganeshn-desktop) (gcc version 4.3.5 (ADI/svn-4960) ) #88 Wed Jun 22 12:23:32 IST 2011

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 32MB

Kernel Managed Memory: 32MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x000a8698

  rodata    = 0x000a8698-0x000e85d8

  bss       = 0x000e9000-0x000f76d0

  data      = 0x000f76e0-0x00104000

    stack   = 0x00102000-0x00104000

  init      = 0x00104000-0x005fe000

  available = 0x005fe000-0x01f00000

  DMA Zone  = 0x01f00000-0x02000000

Hardware Trace Active and Enabled

Boot Mode: 6

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF531 Rev 0.3

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 294 MHz core clock and 98 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 7874

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=24576000 earlyprintk=serial,uart0,115200 console=ttyBF0,115200

PID hash table entries: 128 (order: -3, 512 bytes)

Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)

Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)

Memory available: 25320k/32768k RAM, (5096k init code, 669k kernel code, 367k data, 1024k dma, 292k reserved)

Hierarchical RCU implementation.

NR_IRQS:81

Configuring Blackfin Priority Driven Interrupts

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 585.72 BogoMIPS (lpj=1171456)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Instruction SRAM: 16 KB (4 KB free)

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@5

Switching to clocksource bfin_cs_cycles

msgmni has been set to 49

io scheduler noop registered

io scheduler cfq registered (default)

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 21) is a BFIN-UART

bfin-sport-uart: Blackfin uart over sport driver

bfin-sport-uart.1: ttySS1 at MMIO 0xffc00900 (irq = 18) is a BFIN-SPORT-UART

brd: module loaded

m25p80 spi0.2: found w25Q128, expected m25p64

m25p80 spi0.2: w25Q128 (16384 Kbytes)

Creating 3 MTD partitions on "m25p80":

0x000000000000-0x000000040000 : "bootloader(spi)"

0x000000040000-0x0000001c0000 : "linux kernel(spi)"

0x0000001c0000-0x000001000000 : "file system(spi)"

m25p80 spi0.4: found w25Q128, expected m25p64

m25p80 spi0.4: w25Q128 (16384 Kbytes)

Creating 3 MTD partitions on "m25p80":

0x000000000000-0x000000040000 : "config"

0x000000040000-0x000000c40000 : "Dual rootfs"

0x000000c40000-0x000001000000 : "audio file"

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

dma_alloc_init: dma_page @ 0x014a8000 - 256 pages at 0x01f00000

Freeing unused kernel memory: 5096k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.16.2 (2011-06-22 12:05:59 IST) hush - the humble shell

 

root:/> init: /sbin/syslogd respawning too fast

init: /sbin/syslogd respawning too fast

init: /sbin/syslogd respawning too fast

init: /sbin/syslogd respawning too fast

init: /sbin/syslogd respawning too fast

init: /sbin/syslogd respawning too fast

 

QuoteReplyEditDelete

 

 

2011-06-22 10:30:24     Re: nit: /sbin/syslogd respawning too fast - MSG in 2010R

Mike Frysinger (UNITED STATES)

Message: 101568   

 

please read the faq:

  docs.blackfin.uclinux.org/doku.php?id=faq

Attachments

    Outcomes