2011-06-12 13:02:54     uCasterisk BF533-STAMP problem

Document created by Aaronwu Employee on Aug 27, 2013
Version 1Show Document
  • View in full screen mode

2011-06-12 13:02:54     uCasterisk BF533-STAMP problem

Łukasz Nowakowski (POLAND)

Message: 101222   

 

Hello,

 

I'm trying to run uClinux (version 2006R1), modified with uCasterisk-0.1.7 on my BF533-STAMP to use 1 FXS-port module. Unfortunately when I try uCasterisk scripts or "make bin" command, I always get such an error msg on my STAMP:

 

Using bfsi.bofsi: version magic '2.6.16.27-ADI-2006R2 gcc-4.1' should be '2.6.16.11.ADI-2006R1blackfin gcc-3.4'

insmod: cannot insert `': Invalid module format (-1): Exec format error

Using zaptel.ko

Zapata Telephony Interface Registered on major 196

Using wcfxs.ko

wcfxs: Unknown symbol _bfsi_sport_init

wcfxs: Unknown symbol _bfsi_sport_close

wcfxs: Unknown symbol _bfsi_spi_read_8_bits

wcfxs: Unknown symbol _bfsi_spi_write_8_bits

wcfxs: Unknown symbol _bfsi_spi_init

wcfxs: Unknown symbol _bfsi_reset

insmod: cannot insert `': Unknown symbol in module (-1): No such file or directory

Notice: Configuration file is /etc/zaptel.conf

line 147: Unable to open master device '/dev/zap/ctl'

No entry for terminal type "dumb";

using dumb terminal settings.

eth0: link up, 100Mbps, full-duplex, lpa 0x45E1

init: Booting to single user mode

 

BusyBox v1.00 (2011.06.12-13:48+0000) Built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:~>

 

Any idea how to solve this problem ?

 

Sincerely,

 

Łukasz Nowakowski

QuoteReplyEditDelete

 

 

2011-06-13 15:20:02     Re: uCasterisk BF533-STAMP problem

Mike Frysinger (UNITED STATES)

Message: 101234   

 

sorry, but that release/project is no longer supported here.  please try the asterisk forums:

  blackfin.uclinux.org/gf/project/asterisk/forum/

QuoteReplyEditDelete

Attachments

    Outcomes