2011-05-02 02:29:09     Features missing from uclinux 2010 version

Document created by Aaronwu Employee on Aug 26, 2013
Version 1Show Document
  • View in full screen mode

2011-05-02 02:29:09     Features missing from uclinux 2010 version

Shyam sundar (INDIA)

Message: 100331   

 

Hello world,

 

I want to use AD73322 audio chip, but I dont see that option to be selected in the make menuconfig.

 

Also there was an option in 2009 version to specify which PF pin to be used for waking up the processor when it is in deep sleep. I dont see this option too.

 

How can I use these options  in 2010?

QuoteReplyEditDelete

 

 

2011-05-02 07:07:27     Re: Features missing from uclinux 2010 version

Shyam sundar (INDIA)

Message: 100335   

 

Hello world,

 

Why have been the above features moved to patch?

QuoteReplyEditDelete

 

 

2011-05-02 12:58:33     Re: Features missing from uclinux 2010 version

Mike Frysinger (UNITED STATES)

Message: 100343   

 

you use the general wake up api now:

  docs.blackfin.uclinux.org/doku.php?id=power_management_support#cause_wakeup_event_by_interrupt

QuoteReplyEditDelete

 

 

2011-05-02 23:20:26     Re: Features missing from uclinux 2010 version

Sonic Zhang (CHINA)

Message: 100350   

 

Because the ALSA based driver is obsolette and will be replaced by ASOC based one someday.

Attachments

    Outcomes