2011-04-13 10:24:53     regd drivers fro ADC AD7606 & nanoDAC AD5664R

Document created by Aaronwu Employee on Aug 26, 2013
Version 1Show Document
  • View in full screen mode

2011-04-13 10:24:53     regd drivers fro ADC AD7606 & nanoDAC AD5664R

Ashish Gupta (INDIA)

Message: 99817   

 

Hi,

 

We need to use ADC AD7606 and nanoDAC 5664R with our BF527 based platform - TLL6527m, i looked at the list of drivers here:

 

  docs.blackfin.uclinux.org/doku.php?id=adi_peripheral_drivers

 

and also here:

 

  docs.blackfin.uclinux.org/doku.php?id=linux-kernel:drivers&s[]=drivers

 

1. The ADI nanoDAC AD5664R is listed in the taks sets, I was wondering about the status of the same. If its currently under development, when is it expected to be completed?

 

2. We are planning to use AD7606 ADC for our platform and I didn't see it listed in the above pages, I am assuming a driver for that does not exist, is it in the pipeline to be developed anytime soon? If not, we will plan to develop a driver for community use, what would you suggest should be our starting point for the same?

 

 

 

regards,

 

Ashish

QuoteReplyEditDelete

 

 

2011-04-13 10:38:00     regd drivers fro ADC AD7606 & nanoDAC AD5664R

Michael Hennerich (GERMANY)

Message: 99818    Both drivers are done.

 

AD7606:

  wiki.analog.com/software/driver/linux/ad7606

 

AD5664:

  wiki.analog.com/software/driver/linux/ad5664r

 

The AD7606 driver should be in svn/trunk.

 

However the most recent version as well as the AD5664 exit in

Greg's staging-next git.

 

  git.kernel.org/?p=linux/kernel/git/gregkh/staging-2.6.git;a=shortlog;h=refs/heads/staging-next

 

-Michael

Attachments

    Outcomes