2011-03-02 10:35:23     ADP5588 driver usage documentation / starting point

Document created by Aaronwu Employee on Aug 26, 2013
Version 1Show Document
  • View in full screen mode

2011-03-02 10:35:23     ADP5588 driver usage documentation / starting point

Ashish Gupta (INDIA)

Message: 98594   

 

Hi,

 

I wanted to use the ADP5588 GPIO expander and need to look at the starting point documentation for adding support for it in my BF527 based board's platform file.

 

>Is there a sample platform file? (i looked at ezkit.c and ezbrd.c)

 

> Wiki link to tutorial? I searched the documentation wiki which came up with this link :   docs.blackfin.uclinux.org/doku.php?id=linux-kernel:drivers:adp5588. However this link says that the page has moved to this link   wiki-analog.com/adp5588 - which never loads

 

If not, any similar device that I can take as starting point.

 

Regards

 

Ashish

QuoteReplyEditDelete

 

 

2011-03-02 10:52:37     ADP5588 driver usage documentation / startingpoint

Michael Hennerich (GERMANY)

Message: 98596    >

The documentation moved -

 

Take a look here:

 

  wiki.analog.com/software/driver/linux/adp5588-gpio

 

and here:

 

  wiki.analog.com/software/driver/linux/adp5588

 

There is also sample platform file information included.

 

Regards,

Michael

QuoteReplyEditDelete

 

 

2011-03-18 03:02:29     Re: ADP5588 driver usage documentation / startingpoint

chaitu Krishna (INDIA)

Message: 99025   

 

any one can provide me hardware connections with adp 5588 with blackfin processor

QuoteReplyEditDelete

 

 

2011-03-18 03:07:27     Re: ADP5588 driver usage documentation / startingpoint

Mike Frysinger (UNITED STATES)

Message: 99026   

 

unless i missed something, it's simple I2C and two GPIO lines.  what other info could you possibly need ?

 

did you try reading the wiki page Michael already posted ?

QuoteReplyEditDelete

 

 

2011-03-21 05:29:06     Re: ADP5588 driver usage documentation /startingpoint

Michael Hennerich (GERMANY)

Message: 99088    Please read the documentation I pointed to.

 

  wiki.analog.com/software/driver/linux/adp5588#hardware_configuration

Attachments

    Outcomes