2011-02-18 09:11:14     init: exec rc failed error while kernel image bootup

Document created by Aaronwu Employee on Aug 26, 2013
Version 1Show Document
  • View in full screen mode

2011-02-18 09:11:14     init: exec rc failed error while kernel image bootup

Karthikeyan Jeevanandam (INDIA)

Message: 98255   

 

Hi,

 

To my knowledge I've done all kernel and user configs properly for target BF527 and compiled using 2010 kernel(blackfin-linux-dist-2010R1-RC5)  and 2010 tool chain (blackfin-toolchain-2010R1-RC4.i386 & blackfin-toolchain-uclibc-full-2010R1-RC4) . Compilation is successful and kernel images are created.When the created kernel (uImage.gz.initramfs) is booted in my target "init: exec rc failed error" displayed and stopped further exectution.

 

With the same settings 2009 kernel boots and works properly  for the same target.Please let me know if anything needs to be setted

QuoteReplyEditDelete

 

 

2011-02-18 10:52:01     Re: init: exec rc failed error while kernel image bootup

Mike Frysinger (UNITED STATES)

Message: 98259   

 

find out what file format  your /bin/busybox is and make sure you've enabled the appropriate binfmts in the kernel.  if you're using FDPIC but disabled FDPIC support, then it isnt going to work.  or if you dont have the FDPIC libs installed into /lib/.

QuoteReplyEditDelete

 

 

2011-02-18 13:40:06     Re: init: exec rc failed error while kernel image bootup

Karthikeyan Jeevanandam (INDIA)

Message: 98260   

 

verified the file formats and it is proper.

Loading: #################################################################

         #################################################################

         #################################################################

         #######

done

Bytes transferred = 2953625 (2d1199 hex)

## Booting kernel from Legacy Image at 00000000 ...

   Image Name:   bf527-2.6.34.7-ADI-2010R1

   Created:      2011-02-18 11:29:53 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    2953561 Bytes = 2.8 MB

   Load Address: 00180000

   Entry Point: 004423ec

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 004423ec

console [ttyBF1] enabled, bootconsole disabled

Calibrating delay loop... 1040.38 BogoMIPS (lpj=520192)

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (5 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (40 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

ezkit_init(): registering device resources

bio: create slab <bio-0> at 0

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

msgmni has been set to 111

alg: No test for stdrng (krng)

io scheduler noop registered (default)

ili9322 LCD Driver Initialised

 

adau1361 register major 246

Initial clk tick count 5546214910

mci900_pwm /dev entries driver

mci900_pwm driver initialized successfully

mci900_ad7999 /dev entries driver

mci900_ad7999 driver initialized successfully

bfin-otp: initialized

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 29) is a BFIN-UART

bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART

brd: module loaded

loop: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=25)@sclk=131MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

r8a66597_hcd: driver r8a66597_hcd, 2009-05-26

r8a66597: reg access fail.

usbcore: registered new interface driver usbtmc

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

usbcore: registered new interface driver libusual

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

i2c /dev entries driver

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2008-04-01 05:42:30 UTC (1207028550)

Freeing unused kernel memory: 3624k freed

init: exec rc failed

init: Booting to sin

QuoteReplyEditDelete

 

 

2011-02-19 16:07:52     Re: init: exec rc failed error while kernel image bootup

Mike Frysinger (UNITED STATES)

Message: 98266   

 

are you sure you're actually compiling with the 2010R1 toolchain and dont have an older one in your PATH ?

 

post the output of: ls -Rl romfs/

 

run `make bugreport` and post the tarball as an attachment

Attachments

    Outcomes