2011-01-15 15:46:04     drivers/char/test/built-in.o: No such file: No such file or directory

Document created by Aaronwu Employee on Aug 26, 2013
Version 1Show Document
  • View in full screen mode

2011-01-15 15:46:04     drivers/char/test/built-in.o: No such file: No such file or directory

Carl Berglund (SWEDEN)

Message: 97469   

 

Hi, im trying to add the simple-gpio.c driver to linux kernel and I follow the guide in   docs.blackfin.uclinux.org/doku.php?id=basic_driver_configure_and_build

 

But when i compile i get the error:

 

/opt/uClinux/bfin-uclinux/bin/../bfin-uclinux/bin/ld.real: drivers/char/test/built-in.o: No such file: No such file or directory

make[3]: *** [drivers/char/built-in.o] Error 1

make[2]: *** [drivers/char] Error 2

make[1]: *** [drivers] Error 2

make[1]: Leaving directory `blackfin-linux-dist/linux-2.6.x'

make: *** [linux] Error 1

 

What is built-in.o and how do i get it?

QuoteReplyEditDelete

 

 

2011-01-15 15:55:56     Re: drivers/char/test/built-in.o: No such file: No such file or directory

Mike Frysinger (UNITED STATES)

Message: 97470   

 

use the GPIO sysfs driver:

  docs.blackfin.uclinux.org/doku.php?id=linux-kernel:drivers:gpio-sysfs

QuoteReplyEditDelete

 

 

2011-01-16 09:23:28     Re: drivers/char/test/built-in.o: No such file: No such file or directory

Carl Berglund (SWEDEN)

Message: 97474   

 

Thanks, that works great.

 

But why doesn't the other driver work?

 

And what is the difference between devices in /dev and /sys?

QuoteReplyEditDelete

 

 

2011-01-16 12:22:09     Re: drivers/char/test/built-in.o: No such file: No such file or directory

Mike Frysinger (UNITED STATES)

Message: 97478   

 

there is probably a bug in the way you tried to integrate the code

 

/dev is a bunch of device nodes manually managed while /sys is a pseudo filesystem generated on the fly

Attachments

    Outcomes