2011-01-12 06:32:03     squid proxy:Unable to open configuration file: /etc/config/squid.conf:

Document created by Aaronwu Employee on Aug 26, 2013
Version 1Show Document
  • View in full screen mode

2011-01-12 06:32:03     squid proxy:Unable to open configuration file: /etc/config/squid.conf:

parashuram lamani (INDIA)

Message: 97395   

 

hello,

 

I am trying to run squid on blackfin BF537 stamp board, I enabled squid application using 'make menuconfig' in network application/squid after that 'make' to compile and produce kernel image.

 

I download the uImage to blackfin BF537 stamp board. squid executable is present in the root:/bin> directory

 

when I give './squid' command to run the squid application to test it, it's giving the fallowing error.

 

 

 

FATAL: Unable to open configuration file: /etc/config/squid.conf: (2) No such fi

le or directory

Squid Cache (Version 2.5.STABLE10): Terminated abnormally.

CPU Usage: 0.052 seconds = 0.012 user + 0.040 sys

Maximum Resident Size: 0 KB

Page faults with physical i/o: 0

ABRT

 

how to overcome this error please help me out. I am new to uClinux - blackfin

 

Thanks a lot,

 

Parashuram

QuoteReplyEditDelete

 

 

2011-01-12 11:41:29     Re: squid proxy:Unable to open configuration file: /etc/config/squid.conf:

Mike Frysinger (UNITED STATES)

Message: 97402   

 

we dont have any squid documentation.  please refer to the documentation in the squid source directory, or review the upstream website.

Attachments

    Outcomes