2011-01-07 17:32:32     incorrect image information for uImage-BF526-EZBRD-2010R1-RC5?

Document created by Aaronwu Employee on Aug 26, 2013
Version 1Show Document
  • View in full screen mode

2011-01-07 17:32:32     incorrect image information for uImage-BF526-EZBRD-2010R1-RC5?

Matt Prewett (UNITED STATES)

Message: 97263   

 

I downloaded uImage-BF526-EZBRD-2010R1-RC5 from your website today. When I load this in u-boot and get the info it seems to be for BF527 rather than BF526:

 

***********************

 

bfin> iminfo

 

## Checking Image at 01000000 ...

   Legacy image found

   Image Name:   bf527-2.6.34.7-ADI-2010R1

   Created:      2010-11-29   9:28:19 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    4137460 Bytes = 3.9 MiB

   Load Address: 00001000

   Entry Point:  001f46bc

   Verifying Checksum ... OK

 

***********************

 

 

 

Can you confirm that this image was compiled for BF526 (and not BF527)?

 

-Matt

QuoteReplyEditDelete

 

 

2011-01-07 17:40:24     Re: incorrect image information for uImage-BF526-EZBRD-2010R1-RC5?

Mike Frysinger (UNITED STATES)

Message: 97264   

 

the image name contains the architecture variant, not the exact cpu variant.  so the output you show isnt a problem.

QuoteReplyEditDelete

 

 

2011-01-09 22:14:12     Re: incorrect image information for uImage-BF526-EZBRD-2010R1-RC5?

Sonic Zhang (CHINA)

Message: 97286   

 

Could your bf526 ezbrd boot properly with this image? The correct cpu name should be displayed by dmesg.

QuoteReplyEditDelete

Attachments

    Outcomes