2010-12-14 09:15:02     UART1 PORTG Console problems

Document created by Aaronwu Employee on Aug 25, 2013
Version 1Show Document
  • View in full screen mode

2010-12-14 09:15:02     UART1 PORTG Console problems

Appalayagari Sreedhar (INDIA)

Message: 96708   

 

Hi,

 

I am working with 2009R1-RC1 distribution, BF527 based custom board.

 

The debug console (UART1) is interfaced to the PortG UART1 (PG12 and PG13).

 

I got the uboot up( with some code modifications, i have posted a query to the uboot group i am waiting for their details)

 

and trying to load and run the builded image, junk is displayed on the console.

 

I have selected the PORTG for uart1under BF527 Specific Configuration

 

*** Alternative Multiplexing Scheme ***

 

  │ │                          SPORT0 (PORT G)  --->                                                                 

 

  │ │                          SPORT0 TSCLK Location (PORT PG10)  --->                           

 

  │ │                          UART1 (PORT G)  --->                                                                  

 

  │ │                          NAND (NFC) Data (PORT H)  --->                                              

 

  │ │                          *** Interrupt Priority Assignment ***                                           

 

  │ │                          Priority  --->

 

 

 

Is there anything i missing, can u please help me in resolving the problem.

 

Thank you.

QuoteReplyEditDelete

 

 

2010-12-14 10:22:11     Re: UART1 PORTG Console problems

Mike Frysinger (UNITED STATES)

Message: 96712   

 

are you sure the baud rate is correct ?  if the pin mappings were incorrect, you most likely wouldnt see anything on the console at all.

Attachments

    Outcomes