2010-12-04 05:10:00     can't execute 'boa'

Document created by Aaronwu Employee on Aug 23, 2013
Version 1Show Document
  • View in full screen mode

2010-12-04 05:10:00     can't execute 'boa'

sum max (CHINA)

Message: 96468   

 

1. Login prompt is not correct

 

/ # ls

 

profile Content:

 

# Common login shell init code

PS1='\u:\w> '

 

2. Starting method nfsroot, running tips

 

/bin # boa

sh: can't execute 'boa': No such file or directory

/bin # ./boa

sh: can't execute './boa': Permission denied

 

 

Help me, thank you!

TranslateQuoteReplyEditDelete

 

 

2010-12-04 05:33:42     Re: can't execute 'boa'

Mike Frysinger (UNITED STATES)

Message: 96470   

 

make sure you've actually set +x perms on the file

 

what version of software exactly are you using ?

QuoteReplyEditDelete

 

 

2010-12-04 07:34:54     Re: can't execute 'boa'

sum max (CHINA)

Message: 96471   

 

Thank you for your answer!

 

I'm sure the share dir  "romfs" and file perms (root)777 ,

 

But use "who" can not find the user! the result  the empty!

 

software version linux-dist-2010R1-RC4

TranslateQuoteReplyEditDelete

 

 

2010-12-04 07:57:41     Re: can't execute 'boa'

Mike Frysinger (UNITED STATES)

Message: 96472   

 

i'm not talking about the directory, i'm talking about the file named "boa".  it clearly says "permission denied".

 

what board are you building things for ?  the default ADI build should always have the default prompt setup.  but if you changed things (either in your busybox config or elsewhere), then you need to fix that.

QuoteReplyEditDelete

Attachments

    Outcomes