2010-09-15 01:26:47     Telnet in uclinu

Document created by Aaronwu Employee on Aug 22, 2013
Version 1Show Document
  • View in full screen mode

2010-09-15 01:26:47     Telnet in uclinu

shreya Ban (INDIA)

Message: 93442   

 

Hi,

 

Can anybody tell me how to enable SSH/telnet in uclinux.

QuoteReplyEditDelete

 

 

2010-09-15 01:47:59     Re: Telnet in uclinu

Aaron Wu (CHINA)

Message: 93443   

 

make menuconfig --> Kernel/Library/Defaults Selection -->Customize Application/Library Settings -->Network Applications

QuoteReplyEditDelete

 

 

2010-09-17 00:01:45     Re: Telnet in uclinu

shreya Ban (INDIA)

Message: 93518   

 

I am able to telnet and ping  from board  but there is problem with development system (PC)(linux)

 

How to enable in System?

QuoteReplyEditDelete

 

 

2010-09-17 00:11:17     Re: Telnet in uclinu

Mike Frysinger (UNITED STATES)

Message: 93519   

 

what exactly are you talking about ?  what is your problem ?  what do you want to enable ?

QuoteReplyEditDelete

 

 

2010-09-17 06:59:07     Re: Telnet in uclinu

shreya Ban (INDIA)

Message: 93554   

 

I have BF537 board ,have ported uclinux  on it and a linux System..I want to establish ppp connection between both of them.

 

And i want to telnet to board from Linux computer.

 

I have compiled kernel as per the document below.And have added the required Config files too.

 

  docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:ppp

 

I am able to ping from board to system's IP address.But when i do the same from System to board,its not reachable.

 

and when i run pppd command in system ,the connection gets terminated

 

Linuxcomputer#pppd

 

Using interface ppp0

 

Connect: ppp0 <--> /dev/ttyS0

 

LCP:timeout sending Config-Requests

 

Connection termninated

 

Modem Hang-up.

Attachments

    Outcomes