2010-09-14 19:44:47     missing /dev/input

Document created by Aaronwu Employee on Aug 22, 2013
Version 1Show Document
  • View in full screen mode

2010-09-14 19:44:47     missing /dev/input

Rob Maris (GERMANY)

Message: 93438   

 

I'm missing /dev/input. I have activated gpio-keys and event interface. I checked also the troubleshooting section of

 

  docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:dev-management&s[]=static&s[]=device

 

It is even not present when I select static device configuration (while mdev active, so dynamic generation using evice_table.txt. I don't know where to look now. I cannot use event_test to check events now.

QuoteReplyEditDelete

 

 

2010-09-14 20:20:27     Re: missing /dev/input

Rob Maris (GERMANY)

Message: 93439   

 

When I restore gpio-keys to be loaded on boot time, the event device is present (/dev/event0). Do I need hotplugging feature when gpio-keys build as module?

QuoteReplyEditDelete

 

 

2010-09-14 20:59:34     Re: missing /dev/input

Mike Frysinger (UNITED STATES)

Message: 93440   

 

if you dont have hotplugging enabled, then devices will not be created on the fly.  it'll be up to you to take care of it.

Attachments

    Outcomes